I.MX6Q black screen after power up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q black screen after power up

1,528件の閲覧回数
olafbähring
Contributor I

We are using u-boot and VxWorks7 on a iMX6 Q or DL processor. As display we use a screen either connected to HDMI or LVDS at a resolution of 1376x768. The display works fine when the processor is cold.
When the board is at normal temperature and a power off/on cycle is done, sometimes u-boot and the application is running, but the display keeps black in u-boot and/or in kernel. In some cases u-boot produces a splash screen, but the kernel GUI fails. In this case the IPU VSYNC irq 38 is missing.
When checking the IPU registers in error case of u-boot, we found, that some registers look different:

                                          good    failing
IPU1_SRM_PRI2.DP_S_SRM_MODE                    0        1
IPU1_DP_COM_CONF_SYNC.DP_GWAM_SYNC            0        1
IPU1_DP_Graph_Wind_CTRL_SYNC.DP_GWAV_SYNC    0        80
IPU1_DC_STAT.DC_TRIPLE_BUF_CNT_FULL_0       1       0
IPU1_DC_STAT.DC_TRIPLE_BUF_CNT_EMPTY_0      0       1
IPU1_DC_STAT.DC_TRIPLE_BUF_DATA_FULL_0      1       0
IPU1_DC_STAT.DC_TRIPLE_BUF_DATA_EMPTY_0     0       1
IPU1_DMFC_STAT.DMFC_FIFO_EMPTY_i  i=6       0       1

It seems, that no frames are generated and the IPU is not working at all. What can couse this misbehaviour ? Where should I have a look to ? The configuration is always thee same.

good case:
pixclock = 75386000l Hz
panel size = 1376 x 768
pixel clk = 75386000
setup_disp_channel2: 95ffcff 1376 768 2752 8d5918a0 8d7958a0
bpp_to_pixfmt: 16
initializing idma ch 23 @ 027005c0
IPU DMFC DP HIGH RES: 1(0,1), 5B(2~5), 5F(6,7)
ch 23 word 0 - 00000000 00000000 00000000 E0001800 000BFCAB
ch 23 word 1 - 91AF2B14 02356462 20E3C000 F2C2AFC0 00082CA0
PFS 0x7, BPP 0x3, NPB 0xf
FW 1375, FH 767, Stride 2751
Width0 4+1, Width1 5+1, Width2 4+1, Width3 7+1, Offset0 0, Offset1 5, Offset2 11, Offset3 16
clk_enable pixel_clk usecount 0
IPU_CONF =      0x00000660
IDMAC_CONF =    0x0000002F
IDMAC_CHA_EN1 =         0x00800000
IDMAC_CHA_EN2 =         0x00000000
IDMAC_CHA_PRI1 =        0x18800000
IDMAC_CHA_PRI2 =        0x00000000
IPU_CHA_DB_MODE_SEL0 =  0x00800000
IPU_CHA_DB_MODE_SEL1 =  0x00000000
DMFC_WR_CHAN =          0x00000090
DMFC_WR_CHAN_DEF =      0x202020F6
DMFC_DP_CHAN =          0x0000968A
DMFC_DP_CHAN_DEF =      0x2020F6F6
DMFC_IC_CTRL =          0x00000002
IPU_FS_PROC_FLOW1 =     0x00000000
IPU_FS_PROC_FLOW2 =     0x00000000
IPU_FS_PROC_FLOW3 =     0x00000000
IPU_FS_DISP_FLOW1 =     0x00000000
IPU_INT_STAT[0] =       0x00800000
IPU_INT_STAT[1] =       0x00000000
IPU_INT_STAT[2] =       0x00800000
IPU_INT_STAT[3] =       0x00000000
IPU_INT_STAT[4] =       0x00000000
IPU_INT_STAT[5] =       0x00000000
IPU_INT_STAT[6] =       0x00800000
IPU_INT_STAT[7] =       0x00000000
IPU_INT_STAT[8] =       0x00000000
IPU_INT_STAT[9] =       0x00000000
IPU_INT_STAT[10] =      0x00000000
IPU_INT_STAT[11] =      0x00000000
IPU_INT_STAT[12] =      0x00800000
IPU_INT_STAT[13] =      0x00000000
IPU_INT_STAT[14] =      0x00FF400C
IPU_SRM_PRI2 =          0x06050803
IPU_SRM_STAT =  0x00000000
IPU_TRIPLE_CUR_BUF_0 =  0x00000000
IPU_TRIPLE_CUR_BUF_1 =  0x00004000
IPU_PROC_TASKS_STAT =   0x00000000
IPU_DISP_TASKS_STAT =   0x00000000
IPU_DI0_GENERAL =       0x00300000
IPU_DI0_STAT =  0x00000001
IPU_DI1_GENERAL =       0x00200000
IPU_DI1_STAT =  0x00000005
IPU_DC_STAT =   0x000000A5
IPU_DMFC_GENERAL1 =     0x00000003
IPU_DMFC_GENERAL2 =     0x00000000
IPU_DMFC_STAT =         0x20200020
DI0 OK
Framebuffer at 0x8d5918a0


error case:
pixclock = 75386000l Hz
panel size = 1376 x 768
pixel clk = 75386000
setup_disp_channel2: 95ffcff 1376 768 2752 8d5918a0 8d7958a0
bpp_to_pixfmt: 16
initializing idma ch 23 @ 027005c0
IPU DMFC DP HIGH RES: 1(0,1), 5B(2~5), 5F(6,7)
ch 23 word 0 - 00000000 00000000 00000000 E0001800 000BFCAB
ch 23 word 1 - 91AF2B14 02356462 20E3C000 F2C2AFC0 00082CA0
PFS 0x7, BPP 0x3, NPB 0xf
FW 1375, FH 767, Stride 2751
Width0 4+1, Width1 5+1, Width2 4+1, Width3 7+1, Offset0 0, Offset1 5, Offset2 11, Offset3 16
IPU_CONF =      0x00000660
IDMAC_CONF =    0x0000002F
IDMAC_CHA_EN1 =         0x00800000
IDMAC_CHA_EN2 =         0x00000000
IDMAC_CHA_PRI1 =        0x18800000
IDMAC_CHA_PRI2 =        0x00000000
IPU_CHA_DB_MODE_SEL0 =  0x00800000
IPU_CHA_DB_MODE_SEL1 =  0x00000000
DMFC_WR_CHAN =          0x00000090
DMFC_WR_CHAN_DEF =      0x202020F6
DMFC_DP_CHAN =          0x0000968A
DMFC_DP_CHAN_DEF =      0x2020F6F6
DMFC_IC_CTRL =          0x00000002
IPU_FS_PROC_FLOW1 =     0x00000000
IPU_FS_PROC_FLOW2 =     0x00000000
IPU_FS_PROC_FLOW3 =     0x00000000
IPU_FS_DISP_FLOW1 =     0x00000000
IPU_INT_STAT[0] =       0x00000000
IPU_INT_STAT[1] =       0x00000000
IPU_INT_STAT[2] =       0x00000000
IPU_INT_STAT[3] =       0x00000000
IPU_INT_STAT[4] =       0x00000000
IPU_INT_STAT[5] =       0x00000000
IPU_INT_STAT[6] =       0x00000000
IPU_INT_STAT[7] =       0x00000000
IPU_INT_STAT[8] =       0x00000000
IPU_INT_STAT[9] =       0x00000000
IPU_INT_STAT[10] =      0x00000000
IPU_INT_STAT[11] =      0x00000000
IPU_INT_STAT[12] =      0x00000000
IPU_INT_STAT[13] =      0x00000000
IPU_INT_STAT[14] =      0x00000000
IPU_SRM_PRI2 =          0x0605080B
IPU_SRM_STAT =  0x00000000
IPU_TRIPLE_CUR_BUF_0 =  0x00000000
IPU_TRIPLE_CUR_BUF_1 =  0x00004000
IPU_PROC_TASKS_STAT =   0x00000000
IPU_DISP_TASKS_STAT =   0x00000000
IPU_DI0_GENERAL =       0x00300000
IPU_DI0_STAT =  0x00000001
IPU_DI1_GENERAL =       0x00200000
IPU_DI1_STAT =  0x00000005
IPU_DC_STAT =   0x000000AA
IPU_DMFC_GENERAL1 =     0x00000003
IPU_DMFC_GENERAL2 =     0x00000000
IPU_DMFC_STAT =         0x20200020
DI0 not working
Framebuffer at 0x8d5918a0

ラベル(1)
0 件の賞賛
2 返答(返信)

1,166件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Olaf

to verify if issue is not caused by ddr/power problems, may be recommended to run ddr test

i.MX6/7 DDR Stress Test Tool V2.70 

and verify and reintegrate to VxWorks if needed, logo patches from link

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,166件の閲覧回数
olafbähring
Contributor I

Hi igor,

thank you for the immediate reply.

We have checked the DDR ram settings and it was quite ok. Also the power measurement did not show an inconsistency.

Than we found an errata and also an engineering bulletin EB821 “LDB Clock Switch Procedure & i.MX6 Asynchronous Clock Switching Guidelines”, which handles the clock switching of the display from the MMDC_CH1 clock to PLL5.

This is exactly what we did. The workaround described in the document works fine.

However, thank you for your hints.

Olaf

0 件の賞賛