I.MX6 solox bringup with OTG/SD problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 solox bringup with OTG/SD problem

352件の閲覧回数
liyan1
Contributor I

I have made a board with I.MX6solox. Signal has not been detected on CLK of SD, CLK of SPI after power on. And no activity has been found on DN & DP of USB ether.

PC pointer can be read with trace32 after power on, But the value of PC are always 286C,286A. several registers has been read by JTAG, but the value seems correct.

Is there anyone who can help me?

我用IMX6solox 做了块板子。但上电后SD的CLK、SPI的CLK均没有发现任何信号,USB的DP、DN也没有发现任何信号。 

我用trace32查看了PC指针,PC指针的值总显示为286C和286A。我也通过JTAG读了一些寄存器,也都显示正常。

请给我一些建议。

ラベル(1)
0 件の賞賛
1 返信

280件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 岩 李

one can check board clocks (24MHz, 32.768KHz crystals) if they are stable and

board power supplies using IMX6SXHDG Hardware Development Guide for i.MX 6SoloX

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6SXHDG.pdf

Try nxp official bsps described on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛