Hi,
I was surprised to see that the register map address of I.MX6 solo/dual lite is different from I.MX6 dual/quad.
Maybe I have overlooked something in Freescale documentation, but I didn't see any mentions of that in the docs.
For example looking at the IOMUX register map for PAD SD2_DATA1, I see different addresses:
From i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 0, 11/2012:
From i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 0, 11/2012
20E_0360 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SD2_DATA1)
As for u-boot I can see that only the I.MX6 dual/quad is supported. (from arch/arm/include/asm/arch-mx6/mx6x_pins.h)
MX6Q_PAD_SD2_DAT1__USDHC2_DAT1 = IOMUX_PAD(0x0360, 0x004C, 0, 0x0000, 0, 0),
Am I confused?
If not, is there somewhere a summary of differences? I am worried having to go through the 5000 or so pages of the manual.
Thx a lot,
-jf simon
解決済! 解決策の投稿を見る。
U-boot supports mx6q, dual, dual-lite, solo, solo-lite variants.
Take a look at sabresd board, which supports quad and dual lite variants:
uboot-imx.git - Freescale i.MX u-boot Tree
There is also mx6sl_evk:
U-boot supports mx6q, dual, dual-lite, solo, solo-lite variants.
Take a look at sabresd board, which supports quad and dual lite variants:
uboot-imx.git - Freescale i.MX u-boot Tree
There is also mx6sl_evk: