I.MX6 ULL ADC EXTERNAL MUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 ULL ADC EXTERNAL MUX

546 Views
massimo2
Contributor III

Hello
In i.MX6 ULL manual i havent found ADC muxing into Chaper 4:ext.Signals and Pin Multiplexing.
I saw that it use GPIO inputs.
Have ADC's external pins to be configurated as GPIO with ALT5 mode?

Labels (1)
Tags (4)
0 Kudos
1 Reply

452 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes,the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.Hope it help you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos