Hey everyone,
I'm trying to run a small CEM 1203 buzzer directly from one of the PWMs on my I.MX6. Is there a convenient way to change the period of a pwm-backlight platform device?
Thanks,
L.M.
解決済! 解決策の投稿を見る。
Hi Luke,
You can use this code to allow frequencies in the form of musical "notes" centered around middle-C:
https://github.com/boundarydevices/linux-imx6/commit/63b106e30a42e5ee89c4c7d0644e853f013276db
If you name your platform device "buzzer", you can access the buzzer in sysfs like so:
~/$ echo -n C > /sys/class/leds/buzzer/note # turn on middle C
~/$ echo -n ' ' > /sys/class/leds/buzzer/note # turn it off
Hi Luke,
You can use this code to allow frequencies in the form of musical "notes" centered around middle-C:
https://github.com/boundarydevices/linux-imx6/commit/63b106e30a42e5ee89c4c7d0644e853f013276db
If you name your platform device "buzzer", you can access the buzzer in sysfs like so:
~/$ echo -n C > /sys/class/leds/buzzer/note # turn on middle C
~/$ echo -n ' ' > /sys/class/leds/buzzer/note # turn it off
Hi Eric,
Thanks for the tip, I've updated the leds-pwm.c driver as you suggested but I'm not sure how to register the platform device.
I'm still on kernel 3.0.35 and all the examples I have use leds-gpio or pwm-backlight. I haven't had to add a platform device yet but looking at leds_pwm.h and other platform devices I came up with this:
static struct led_pwm imx6_led_pwms[] = {
{
.name = "buzzer",
.default_trigger = ,
.pwm_id = 2,
.active_low = ,
.max_brightness = ,
.pwm_period_ns = ,
}
};
static struct led_pwm_platform_data imx6q_led_pwms_data = {
.leds = imx6q_pwm_leds,
.num_leds = ARRAY_SIZE(imx6q_led_pwms),
};
static struct platform_device imx6q_pwm_led_device = {
.name = "leds-pwm",
.id = 1,
.num_resources = ,
.dev = {
.platform_data = &imx6q_led_pwms_data,
}
};
static void __init imx6q_add_device_led_pwms(void)
{
platform_device_register(&imx6q_pwm_led_device);
}
Could you help me fill in the blanks? Or point me towards an example?
Hi Luke
please look at sect. 8.6 "Buzzer" below
Linux Software User Manual (i.MX6) - BlueWiki
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------