我想將Uboot燒寫到emmc中,不過我不想用MFGTool而是其他的辦法。
我應該怎樣去實現,怎樣去分區?
我的emmc是THGBMHG7C2LBAU7 (emmc5.1)
麻烦了~
Hi, Ansel Yip
You can flash a u-boot in eMMC with below two methods,
Method - 1: Using UUU tool
Below command will flash u-boot to an eMMC.
Please refer UUU.pdf in this link for more information.
Method - 2: Flash an eMMC from an SD Card
Follow below steps to flash an eMMC from an SD Card:
Hope this will help you.
Regards,
Shivani
i.MX_6_SABRE-SD_Linux_Users_Guide.pdf
我知道这个文档介绍,不过不会用,可以详细教一下吗?
-----------------------------------------------------------------------------------------
U-Boot 2016.03-svn8 (Mar 28 2019 - 14:16:31 +0800)
CPU: Freescale i.MX6QP rev1.1 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 40C
Reset cause: POR
Board: MX6QP-AVM718-MB revV20
I2C: ready
DRAM: 2 GiB
force_idle_bus: sda=1 scl=0 sda.gp=0x6d scl.gp=0x3e
force_idle_bus: failed to clear bus, sda=1 scl=0
MMC: FSL_SDHC: 0, FSL_SDHC: 1
No panel detected: default to HD700-CLAA
Display: HD700-CLAA (1200x800)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0 is current device
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
[abortboot_normal]Hit any key to stop autoboot: