I.MX6 DUAL CORE 32bit mode DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 DUAL CORE 32bit mode DDR

Jump to solution
1,785 Views
BESTFREESCALE
Contributor II

Dear community members,

I reviewed  32-bit DDR Interface using I.MX6 Dual Core but don't decide to use SDRAM_SDCLK0 or SDRAM_SDCLK1 for 32-bit mode.

According to EVM, DRAM_SDCLK_1 was applied to DDR3_D[0:31] ICs , I didn't understood exactly why SDRAM_SDCLK1 was applied to DDR3_D[0:31] ICs instead of SDRAM_SDCLK0.

Q1) If I use DRAM_SDCLK_0 instead of SDRAM_SDCLK1 for 32-bit mode DDR3 ( 2 * ICs) , Is there no problem?

Q2) If I use DRAM_SDCLK_1 for 32-BIT mode DDR3 Interface, Is there no problem?

Could you advice questions for me?

Thank

Labels (6)
0 Kudos
Reply
1 Solution
1,072 Views
Yuri
NXP Employee
NXP Employee

DRAM clock signals SDCLK0 and SDCLK1 are the practically the same (by default) and in this sense do no relate to CS0 or CS1

channels.

View solution in original post

0 Kudos
Reply
1 Reply
1,073 Views
Yuri
NXP Employee
NXP Employee

DRAM clock signals SDCLK0 and SDCLK1 are the practically the same (by default) and in this sense do no relate to CS0 or CS1

channels.

0 Kudos
Reply