I.MX287 UART PPP mxs-auart mxs-auart.0: Unhandled status 520080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX287 UART PPP mxs-auart mxs-auart.0: Unhandled status 520080

1,082件の閲覧回数
qustjinxin
Contributor I

HI,

I want to know how change this for ppp for uart?

/* modem status interrupt bits are undefined
after reset,and the hardware do not support
DSRMIS,DCDMIS and RIMIS bit,so we should ingore
them when they are pending. */
if (istat & (BM_UARTAPP_INTR_ABDIS
| BM_UARTAPP_INTR_OEIS
| BM_UARTAPP_INTR_BEIS
| BM_UARTAPP_INTR_PEIS
| BM_UARTAPP_INTR_FEIS
| BM_UARTAPP_INTR_RTIS
| BM_UARTAPP_INTR_TXIS
| BM_UARTAPP_INTR_RXIS
| BM_UARTAPP_INTR_CTSMIS)) {
dev_info(s->dev, "Unhandled status %x\n", istat);
}
__raw_writel(istatus & (BM_UARTAPP_INTR_ABDIS
| BM_UARTAPP_INTR_OEIS
| BM_UARTAPP_INTR_BEIS
| BM_UARTAPP_INTR_PEIS
| BM_UARTAPP_INTR_FEIS
| BM_UARTAPP_INTR_RTIS
| BM_UARTAPP_INTR_TXIS
| BM_UARTAPP_INTR_RXIS
| BM_UARTAPP_INTR_DSRMIS
| BM_UARTAPP_INTR_DCDMIS
| BM_UARTAPP_INTR_CTSMIS
| BM_UARTAPP_INTR_RIMIS),
s->port.membase + HW_UARTAPP_INTR_CLR);

when i use uart to ppp ,it always print  mxs-auart mxs-auart.0: Unhandled status 520080 !

when i disable this part ,it works ok.

thanks !

ラベル(1)
0 件の賞賛
1 返信

428件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

this is just warning and seems can be safely ignored.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛