I.MX283 LCDIF can supported 1024 x 128 pixed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX283 LCDIF can supported 1024 x 128 pixed?

703 Views
ouuy
Contributor II

in datasheet the i.mx283 lcdif

High display resolutions up to 800x480 supported.

i want to supported 1024 x 128 ,  can support ?

0 Kudos
3 Replies

534 Views
Yuri
NXP Employee
NXP Employee

Display resolution in itself is not a problem for i.MX28 / 23. LCDIF Horizontal and Vertical Valid Data
Count Register (HW_LCDIF_TRANSFER_COUNT) contains 16 bit fields for vertical and horizontal

counters. So,  1024 x 128 may be supported.

   Another point  what is display interface  ?  This should be analyzed first.

The i.MX28  manual says about display resolutions up to 800 x 480.

This restriction mainly concerns performance issue : the i.MX28 is able to drive LCD panel up

to 800x480 resolution at 60Hz.

  Since both pixel pipeline and LCDIF do not impose any hard maximum limit to

800x480, in theory higher resolution LCD panel is allowed.

However, we do not recommend driving any panel with higher resolution than

800x480 due to limited internal bus bandwidth. It is possible to run at a higher

resolution at lower frame rate (800x600 @ 48Hz is the same number of pixels/sec

as 800x480 @ 60Hz).

  This is correct for DOTCLK mode. As for System mode, internal bus bandwidth is

not the problem.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

534 Views
YixingKong
Senior Contributor IV

Ou

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos

534 Views
YixingKong
Senior Contributor IV

Ou

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos