I.MX280 Touch screen controller.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX280 Touch screen controller.

570 Views
russellholmes
Contributor I

Hello all,

Hoping to get a quick and concise answer on this one!

Does the MCIMX280DVM4B come with a touch screen controller interface? I know the MCIMX283DVM4B uses some pins on the LRADC as a touch screen controller.

I was hoping that this is the same for the MCIMX280DVM4B.


Thanks in advance!!

Labels (2)
0 Kudos
1 Reply

470 Views
Yuri
NXP Employee
NXP Employee

  According to Table 2 (i.MX28 Functional Differences) of the i.MX28

Datasheet  (IMX28CEC, Rev. 3, 07/2012) the i.MX280 supports the LRADC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos