Hello
I used a USB hub on i.mx8mini to make 4 usb ports.
By the way, if I use Type-c and usb 2.0 together, I don't know how to configure
i.mx8mini has two USB ports
One used for FW download
The other one will use a 4ch USB hub
But is it okay to connect Type-C and usb 2.0 to this 4ch USB hub?
If there is a problem, please let me know which circuit you can refer to.
Or let me know if there is any way other than 4ch USB hub.
Thank you
Hello Danny,
It´s ok to use it but you need to adapt your USB 2.0 to have type C with the USB 3.0.
Regards
Hello Bio_TICFSL
Can you explain in more detail?
I will connect the USB 2.0 4ch HUB to the other one(i.mx8mini usb port)
And I will configure 4ch HUB as follows
1ch: Type-c connector to connect tablet (type-c to type-c planned)
2ch: USB 2.0 connector
3ch: USB 2.0 connector
4ch: don't care
What should USB 3.0 do in this configuration?
If you have any references data(circuit, doc), please introduce me
Thank you