Hi all,
I consider using i.MX6DL RMII.
Please see Table 23-1 in IMX6SDLRM (Rev.1).
It shows ENET_CRS_DV pad can use for generating the CRS signal in RMII mode.
However, in chapter 37.4.117, there is no description about "CRS".
So I understand I can use ENET_CRS_DV pad to generate CRS in RMII mode with the following setting.
Is my understanding correct?
1. Set MUX_MODE field in chapter 37.4.117 to 001b (ALT1 ENET_RX_EN).
2. Set DAISY bit in chapter 37.4.517 to 0 (ENET_CRS_DV_ALT1).
If some adittional setting is required, could you let me know it?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Yes, you are right.
The RMII port was verified on iMX6 OTT reference design: https://community.freescale.com/docs/DOC-94561
The macro for that pin:
MX6DL_PAD_ENET_CRS_DV__ENET_RX_EN
#define MX6DL_PAD_ENET_CRS_DV__ENET_RX_EN \
IOMUX_PAD(0x05B4, 0x01E4, 1, 0x0828, 0, MX6DL_ENET_PAD_CTRL)
Yes, you are right.
The RMII port was verified on iMX6 OTT reference design: https://community.freescale.com/docs/DOC-94561
The macro for that pin:
MX6DL_PAD_ENET_CRS_DV__ENET_RX_EN
#define MX6DL_PAD_ENET_CRS_DV__ENET_RX_EN \
IOMUX_PAD(0x05B4, 0x01E4, 1, 0x0828, 0, MX6DL_ENET_PAD_CTRL)