How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board 3.14.52

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board 3.14.52

ソリューションへジャンプ
3,033件の閲覧回数
浩卢
Contributor III

hi:

How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board.What should I do with uboot ?

Now I am using  the version yocto 3.14.52.u-boot version is 2015.04.

I have try to do some change like this How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board

ddr change.png

But it doesn't work. It is still 1G size DDR. Here is the log

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Apr 20 2016 - 16:01:47)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 31 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

switch to partitions #0, OK

mmc2(part 0) is current device

Net:   FEC [PRIME]

Error: FEC address not set.

Normal Boot

Hit any key to stop autoboot:  0

ラベル(3)
0 件の賞賛
返信
1 解決策
1,713件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please run ddr test

i.MX6/7 DDR Stress Test Tool V2.52

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

Best regards

igor

元の投稿で解決策を見る

5 返答(返信)
1,713件の閲覧回数
sywksmstkadlfgk
Contributor III

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

1,714件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please run ddr test

i.MX6/7 DDR Stress Test Tool V2.52

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

Best regards

igor

1,713件の閲覧回数
浩卢
Contributor III

Thank you igorpadykov .

0 件の賞賛
返信
1,713件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please use Chapter 1 (Porting U-Boot from an i.MX 6/7 Reference Board to

an i.MX 6/7 Custom Board) of "i.MX_BSP_Porting_Guide.pdf" in Linux docs.

< http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS >

Also, the following may be helpful.

"Freescale i.MX6 DRAM Port Application Guide-DDR3"

< https://community.freescale.com/docs/DOC-101708 >

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,717件の閲覧回数
浩卢
Contributor III

Thank you Yuri Muhin.

0 件の賞賛
返信