Vu, HTML5 is an option to Adobe Flash Player.
For those that are on other platforms starting with Android ICS, the i.MX6 series with VPU hardware does work with a marketplace flash player but still requires Adobe certification before it can be put into production.
I'm sorry, but marketplace Adobe Flash player will be quite slow as it is not hardware accelerated on Gingerbread.
Also Adobe has announced end of life for Adobe Flash Player end of 2011 and Freescale did not support the i.MX53 QSB with the Adobe Flash Player. Adobe has announced plans to remove the Adobe Flash Player from the Android marketplace so it might not be available to download at this point.
If you do find the Adobe Flash Player version then note performance of video will be slow.
Vu, HTML5 is an option to Adobe Flash Player.
For those that are on other platforms starting with Android ICS, the i.MX6 series with VPU hardware does work with a marketplace flash player but still requires Adobe certification before it can be put into production.