How to switch the mode of HDMI TX in i.MX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to switch the mode of HDMI TX in i.MX8M

ソリューションへジャンプ
2,369件の閲覧回数
ko-hey
Senior Contributor II

Hi all

 

I have a question about HDMI TX in i.MX8M.

 

According to the chapter 13.4 of following document, the HD Display Transmitter Controller (HDMI TX) IP supports some protocols and it seems that it can switch by register or software configuration.

https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

 

How can use switch the protocols ?

 

If it can switch by a register, please specify it.

On the other hand, if it can switch the protocol by only software, please provide me a sample source.

 

 

Ko-hey

0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  For a HD Display TX controller supporting multi-protocols, switching

between the two modes (HDMI and DisplayPort) requires reloading the

appropriate FW.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,624件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  For a HD Display TX controller supporting multi-protocols, switching

between the two modes (HDMI and DisplayPort) requires reloading the

appropriate FW.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,623件の閲覧回数
ko-hey
Senior Contributor II

Hi Yuri Muhin

Does it need reset after reloading the FW ?

Ko-hey

0 件の賞賛
返信
1,623件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  HDMI FW, required for HDMI controller should be loaded at i.MX8M boot

stage, without following system reset.

Regards,

Yuri.

0 件の賞賛
返信