How to switch the mode of HDMI TX in i.MX8M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to switch the mode of HDMI TX in i.MX8M

跳至解决方案
2,299 次查看
ko-hey
Senior Contributor II

Hi all

 

I have a question about HDMI TX in i.MX8M.

 

According to the chapter 13.4 of following document, the HD Display Transmitter Controller (HDMI TX) IP supports some protocols and it seems that it can switch by register or software configuration.

https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

 

How can use switch the protocols ?

 

If it can switch by a register, please specify it.

On the other hand, if it can switch the protocol by only software, please provide me a sample source.

 

 

Ko-hey

0 项奖励
回复
1 解答
1,553 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  For a HD Display TX controller supporting multi-protocols, switching

between the two modes (HDMI and DisplayPort) requires reloading the

appropriate FW.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,554 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  For a HD Display TX controller supporting multi-protocols, switching

between the two modes (HDMI and DisplayPort) requires reloading the

appropriate FW.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,553 次查看
ko-hey
Senior Contributor II

Hi Yuri Muhin

Does it need reset after reloading the FW ?

Ko-hey

0 项奖励
回复
1,553 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  HDMI FW, required for HDMI controller should be loaded at i.MX8M boot

stage, without following system reset.

Regards,

Yuri.

0 项奖励
回复