Hi Community,
I'm working on an imx.6 DL board bring-up using BSP l5.0.0_1.0.0-ga.
We need initialize the MMDC in plugin mode, but the parameters such as ivt_header, boot_data in mx6_plugin.S are all set to 0x0 by default.
I have tried to compile and run u-boot with CONFIG_USE_PLUGIN enabled on SabreSD demo board but no success to boot up.
Compared with old flash_header.s of u-boot v-2009, I think the ivt_header, boot_data, app_code_jump_v etc. are missing in l5.0.0_1.0.0-ga and later BSP.
Dose anyone can help to provide these parameters in plugin mode?
Thanks.
Best Regards,
Peter