How to set environment for building u-boot's fw_printenv for i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set environment for building u-boot's fw_printenv for i.MX6Q

5,008 Views
lqll
Contributor III

Hello

My environment is i.MX6Q and Android 4.4.2.

I want to build fw_printenv but get stuck,and this is my steps:

l@workspace-All-Series:~/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx$ make distclean

l@workspace-All-Series:~/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx$ make mx6q_sabresd_android_config

Configuring for mx6q_sabresd_android board...

l@workspace-All-Series:~/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx$ export ARCH=arm

l@workspace-All-Series:~/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx$ export CROSS_COMPILE=~/android-4.4.2_sdi_in/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

l@workspace-All-Series:~/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx$ make env

make -C tools/env all MTD_VERSION= || exit 1

make[1]: Entering directory `/home/l/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx/tools/env'

/home/l/android-4.4.2_sdi_in/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-gcc -Wall -DUSE_HOSTCC -I/home/l/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx/include crc32.c  fw_env.c  fw_env_main.c -o fw_printenv

In file included from crc32.c:14:0:

/home/l/android-4.4.2_sdi_in/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/../lib/gcc/arm-eabi/4.6.x-google/include/stdint.h:3:26: fatal error: stdint.h: No such file or directory

compilation terminated.

fw_env.c:27:19: fatal error: errno.h: No such file or directory

compilation terminated.

fw_env_main.c:42:19: fatal error: stdio.h: No such file or directory

compilation terminated.

make[1]: *** [fw_printenv] Error 1

make[1]: Leaving directory `/home/l/android-4.4.2_sdi_in/bootable/bootloader/uboot-imx/tools/env'

make: *** [env] Error 1

I think I use wrong cross compiler,please help me what can I do.

Thank You

Qiulong Li

Labels (3)
0 Kudos
7 Replies

2,944 Views
hongchao0680
Contributor III

use another cross compile "arm-fsl-linux-gnueabi-" is OK, build cmd like below:

$ make mx6qsabresd_defconfig
$ make CROSS_COMPILE=/opt/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi- env

Tags (1)

2,944 Views
zhanghakwell
Contributor III

I also meet this question, my step is like below:

vmuser@ubuntu:~/imx6/uboot/2016.03-r0$ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi
vmuser@ubuntu:~/imx6/uboot/2016.03-r0$  make mx6sxsabresd_defconfig
  HOSTCC  scripts/basic/fixdep
  HOSTCC  scripts/kconfig/conf.o
  SHIPPED scripts/kconfig/zconf.tab.c
  SHIPPED scripts/kconfig/zconf.lex.c
  SHIPPED scripts/kconfig/zconf.hash.c
  HOSTCC  scripts/kconfig/zconf.tab.o
  HOSTLD  scripts/kconfig/conf
#
# configuration written to .config
#
vmuser@ubuntu:~/imx6/uboot/2016.03-r0$ make
scripts/kconfig/conf  --silentoldconfig Kconfig
  CHK     include/config.h
  UPD     include/config.h
  GEN     include/autoconf.mk
  GEN     include/autoconf.mk.dep
  ......
  OBJCOPY examples/standalone/hello_world.bin
  LDS     u-boot.lds
  LD      u-boot
  OBJCOPY u-boot-nodtb.bin
  COPY    u-boot.bin
  CFGS    board/freescale/mx6sxsabresd/imximage.cfg.cfgtmp
  MKIMAGE u-boot.imx
  OBJCOPY u-boot.srec
  SYM     u-boot.sym
  CFG     u-boot.cfg
vmuser@ubuntu:~/imx6/uboot/2016.03-r0$ make env
  LD      tools/env/built-in.o
  HOSTCC  tools/env/aes.o
In file included from tools/env/aes.c:1:0:
tools/env/../../lib/aes.c:28:20: fatal error: string.h: No such file or directory
compilation terminated.
make[1]: *** [tools/env/aes.o] Error 1
make: *** [env] Error 2
vmuser@ubuntu:~/imx6/uboot/2016.03-r0$

Is there something wrong in this uboot source code?

0 Kudos

2,944 Views
zhanghakwell
Contributor III

use another cross compile "arm-fsl-linux-gnueabi-" is OK, new build cmd like below:

$ make mx6sxsabresd_defconfig
$ make CROSS_COMPILE=/opt/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi- env

but why pre toolchain which build from yocto project 4.1.15-2.0.0ga is not OK?

build cmd like below:

$ bitbake meta-toolchain

or

$ bitbake meta-toolchain-qt5

2,055 Views
billchen
Contributor III

good answer

0 Kudos

2,944 Views
chenqigan_usr
Contributor I

Dear Qiulong Li:

you can compiled fw_printenv with gcc -static option.

eg:

modify $(UBOOT_PATH_TOP)/tools/env/Makefile

pastedImage_1.png

what's more,you should use linux-gnueabi- not for android  provied prebuilts/gcc/linux-x86/arm/arm-linux-androideabi.

eg:

export ARCH=arm

export CROSS_COMPILE=/opt/Embedsky/tq-linaro-toolchain/bin/arm-none-linux-gnueabi-

modify $(UBOOT_PATH_TOP)/tools/env/Makefile

make env 

 

0 Kudos

2,944 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiulong

these are special uboot utilities and its support/building may depend on uboot version.

Please read about its usage on uboot wiki:

HowCanIAccessUBootEnvironmentVariablesInLinux < DULG < DENX

and post possible questions on uboot mail list

U-Boot Info Page

For android 4.4.2 uboot  building it may be useful to look at attached Porting Guide sect.1.2.1

Preparing the Code

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,944 Views
lqll
Contributor III

Hi igor

Thanks for your reply.

My u-boot's version is v2009.08.

The attach file you give me tells me how to  Preparing the Code,I have read and I'm sure my environment is OK,because I can build u-boot.

I can use the follow cmd to build u-boot

make distclean

make mx6q_sabresd_android_config

export ARCH=arm

export CROSS_COMPILE=~/android-4.4.2_sdi_in/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

make

But I can't use the follow cmd to make make fw_printenv

make distclean

make mx6q_sabresd_android_config

export ARCH=arm

export CROSS_COMPILE=~/android-4.4.2_sdi_in/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-

make env

Thanks

Qiulong Li

0 Kudos