Hi,
we do not have USB Type C hardware support, so we do not need software support. Removing the driver and the related device tree entry ends in a non-bootable kernel. What changes have to be done to remove the USB Type C support?
Further infos:
- Custom Board based on imx8mn-ddr4-evk
Best,
Michael
Device Tree based on fsl-imx8mn-ddr4-evk.dts: If the part typec_ptn5110_1 is removed the kernel hangs during bootup.
Removed the following from the defconfig file.
CONFIG_TYPEC_TCPCI
CONFIG_TYPEC_TCPM
Removed these entries from device tree file
pinctrl_typec1: typec1grp {
[..]
};
typec_ptn5110_1: ptn5110@50 { [..] }; typec_ptn5110_2: ptn5110@52 { [..] };
&usbotg1 { [..] };