How to remove PCI interface for WiFi module on i.MX8MQ EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to remove PCI interface for WiFi module on i.MX8MQ EVK

1,112 次查看
limlee
Contributor I

Dear All,

I would like to know how to remove the PCI interface for WiFi module installed by default on i.MX8MQ EVK.

Should I change some configurations for device tree file?

When lspci command is input, PCI information about the WiFi module basically installed is printed as follows.

=============================================================================

U-Boot SPL 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g7ade5b4 (Feb 03 2021 - 08:42:18 +0000)
PMIC: PFUZE100 ID=0x10
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3200MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 3200MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2


U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g7ade5b4 (Feb 03 2021 - 08:42:18 +0000)

CPU: Freescale i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 37C
Reset cause: POR
Model: Freescale i.MX8MQ EVK
DRAM: 3 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
No panel detected: default to HDMI
Display: HDMI (1280x720)
cdn_api_checkalive: keep-alive counter did not increment for 10us...
HDMI enable failed!
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF a-20190
- U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g7ade5b4

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net:
Warning: ethernet@30be0000 MAC addresses don't match:
Address in ROM is 00:04:9f:06:ef:a8
Address in environment is 00:04:9f:05:a6:d5
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
switch to partitions #0, OK
mmc1 is current device
** Unable to read file boot.scr **
22120960 bytes read in 952 ms (22.2 MiB/s)
Booting from mmc ...
44769 bytes read in 17 ms (2.5 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300dee0

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.78-imx_4.14.78_1.0.0_ga (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Wed Feb 3 09:34:40 UTC 2021
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: Freescale i.MX8MQ EVK
[ 0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030860000 (options '115200')
[ 0.000000] bootconsole [ec_imx6q0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000044000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000fdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xfdfbac00-0xfdfbc9ff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000fdffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000fdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000fdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu @ffff8000bdf55000 s57624 r8192 d32488 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 765056
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 2053844K/3108864K available (13244K kernel code, 1442K rwdata, 5568K rodata, 1280K init, 439K bss, 71980K reserved, 983040K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008d70000 ( 13248 KB)
[ 0.000000] .rodata : 0xffff000008d70000 - 0xffff0000092f0000 ( 5632 KB)
[ 0.000000] .init : 0xffff0000092f0000 - 0xffff000009430000 ( 1280 KB)
[ 0.000000] .data : 0xffff000009430000 - 0xffff000009598a00 ( 1443 KB)
[ 0.000000] .bss : 0xffff000009598a00 - 0xffff0000096069e0 ( 440 KB)
[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0002f80000 ( 47 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff8000be000000 ( 3040 MB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] i.MX8MQ clock driver init done
[ 0.000000] arch_timer: cp15 timer(s) running at 8.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.000003] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.008722] system counter timer init
[ 0.011721] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.019709] clocksource: imx sysctr: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.030910] Console: colour dummy device 80x25
[ 0.034485] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333)
[ 0.044746] pid_max: default: 32768 minimum: 301
[ 0.049432] Security Framework initialized
[ 0.054675] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[ 0.061303] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.067797] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.074498] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.097695] ASID allocator initialised with 32768 entries
[ 0.105697] Hierarchical SRCU implementation.
[ 0.114165] Cannot find MU entry in device tree
[ 0.115968] CPU identified as i.MX8MQ, silicon rev 2.1
[ 0.121785] EFI services will not be available.
[ 0.133553] smp: Bringing up secondary CPUs ...
[ 0.161711] Detected VIPT I-cache on CPU1
[ 0.161737] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.161760] CPU1: Booted secondary processor [410fd034]
[ 0.189760] Detected VIPT I-cache on CPU2
[ 0.189777] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.189792] CPU2: Booted secondary processor [410fd034]
[ 0.217827] Detected VIPT I-cache on CPU3
[ 0.217844] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.217859] CPU3: Booted secondary processor [410fd034]
[ 0.218069] smp: Brought up 1 node, 4 CPUs
[ 0.267711] SMP: Total of 4 processors activated.
[ 0.272421] CPU features: detected feature: GIC system register CPU interface
[ 0.279571] CPU features: detected feature: 32-bit EL0 Support
[ 0.285413] CPU features: detected feature: Kernel page table isolation (KPTI)
[ 0.322276] CPU: All CPU(s) started at EL2
[ 0.323677] alternatives: patching kernel code
[ 0.329284] devtmpfs: initialized
[ 0.336862] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0
[ 0.343507] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.352450] futex hash table entries: 1024 (order: 5, 131072 bytes)
[ 0.384892] pinctrl core: initialized pinctrl subsystem
[ 0.388633] DMI not present or invalid.
[ 0.391481] NET: Registered protocol family 16
[ 0.399659] cpuidle: using governor menu
[ 0.401471] vdso: 2 pages (1 code @ ffff000008d76000, 1 data @ ffff000009434000)
[ 0.408211] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.421554] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.425820] Serial: AMBA PL011 UART driver
[ 0.436000] imx8mq-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver
[ 0.474085] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.488343] ACPI: Interpreter disabled.
[ 0.490685] vgaarb: loaded
[ 0.492519] SCSI subsystem initialized
[ 0.497037] usbcore: registered new interface driver usbfs
[ 0.501434] usbcore: registered new interface driver hub
[ 0.506976] usbcore: registered new device driver usb
[ 0.513086] i2c i2c-0: IMX I2C adapter registered
[ 0.516378] i2c i2c-0: can't use DMA, using PIO instead.
[ 0.522290] i2c i2c-1: IMX I2C adapter registered
[ 0.526399] i2c i2c-1: can't use DMA, using PIO instead.
[ 0.532675] i2c i2c-2: IMX I2C adapter registered
[ 0.536444] i2c i2c-2: can't use DMA, using PIO instead.
[ 0.542878] media: Linux media interface: v0.10
[ 0.546355] Linux video capture interface: v2.00
[ 0.551263] pps_core: LinuxPPS API ver. 1 registered
[ 0.555868] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.565143] PTP clock support registered
[ 0.569270] EDAC MC: Ver: 3.0.0
[ 0.572811] dmi: Firmware registration failed.
[ 0.577427] MU is ready for cross core communication!
[ 0.583438] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.587432] imx rpmsg driver is registered.
[ 0.591628] Advanced Linux Sound Architecture Driver Initialized.
[ 0.598231] Bluetooth: Core ver 2.22
[ 0.601016] NET: Registered protocol family 31
[ 0.605403] Bluetooth: HCI device and connection manager initialized
[ 0.611822] Bluetooth: HCI socket layer initialized
[ 0.616648] Bluetooth: L2CAP socket layer initialized
[ 0.621772] Bluetooth: SCO socket layer initialized
[ 0.628142] clocksource: Switched to clocksource arch_sys_counter
[ 0.633020] VFS: Disk quotas dquot_6.6.0
[ 0.636661] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.643719] pnp: PnP ACPI: disabled
[ 0.664221] NET: Registered protocol family 2
[ 0.666253] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[ 0.673347] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[ 0.680098] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.686280] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[ 0.692255] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[ 0.698839] NET: Registered protocol family 1
[ 0.703935] RPC: Registered named UNIX socket transport module.
[ 0.708958] RPC: Registered udp transport module.
[ 0.713611] RPC: Registered tcp transport module.
[ 0.718317] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.726202] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.733227] kvm [1]: 8-bit VMID
[ 0.736533] kvm [1]: GICv3: no GICV resource entry
[ 0.740520] kvm [1]: disabling GICv2 emulation
[ 0.745030] kvm [1]: GIC system register CPU interface enabled
[ 0.751167] kvm [1]: vgic interrupt IRQ1
[ 0.755111] kvm [1]: Hyp mode initialized successfully
[ 0.767803] audit: initializing netlink subsys (disabled)
[ 0.770714] audit: type=2000 audit(0.671:1): state=initialized audit_enabled=0 res=1
[ 0.771348] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 0.781213] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.782364] NFS: Registering the id_resolver key type
[ 0.782381] Key type id_resolver registered
[ 0.782384] Key type id_legacy registered
[ 0.782393] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.782411] jffs2: version 2.2. (NAND) ⓒ 2001-2006 Red Hat, Inc.
[ 0.783005] 9p: Installing v9fs 9p2000 file system support
[ 0.802603] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.802608] io scheduler noop registered
[ 0.802761] io scheduler cfq registered (default)
[ 0.802765] io scheduler mq-deadline registered
[ 0.802769] io scheduler kyber registered
[ 0.821929] imx-sdma 30bd0000.sdma: no iram assigned, using external mem
[ 0.824190] imx-sdma 30bd0000.sdma: Falling back to user helper
[ 0.827830] imx-sdma 302c0000.sdma: no iram assigned, using external mem
[ 0.835458] mxs-dma 33000000.dma-apbh: initialized
[ 0.837731] Bus freq driver module loaded
[ 0.839457] Config NOC for VPU and CPU
[ 0.848115] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.851664] SuperH (H)SCI(F) driver initialized
[ 0.852534] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 44, base_baud = 1562500) is a IMX
[ 0.901475] console [ttymxc0] enabled
[ 0.901475] console [ttymxc0] enabled
[ 0.905943] bootconsole [ec_imx6q0] disabled
[ 0.905943] bootconsole [ec_imx6q0] disabled
[ 0.915565] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 45, base_baud = 5000000) is a IMX
[ 0.931166] dcss-core 32e00000.dcss: Configured video pll 2 with ref_clk 1 freq 594000000 (actual 594000000)
[ 0.952101] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 0.958791] [drm] No driver support for vblank timestamp query.
[ 0.964854] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)
[ 2.472148] [drm:hdp_fw_check] *ERROR* CDN_API_General_Test_Echo_Ext_blocking - echo test failed, check firmware!
[ 2.472155] [drm:imx_hdp_imx_bind] *ERROR* Failed to initialise HDP firmware
[ 2.489508] imx-drm display-subsystem: failed to bind 32c00000.hdmi (ops imx_hdp_imx_ops): -6
[ 2.498152] imx-drm display-subsystem: master bind failed: -6
[ 2.511770] loop: module loaded
[ 2.520074] fsl-quadspi 30bb0000.qspi: n25q256a (32768 Kbytes)
[ 2.527779] slram: not enough parameters.
[ 2.535304] libphy: Fixed MDIO Bus: probed
[ 2.540573] NXP PHY: loading NXP PHY driver: [autonomous mode]
[ 2.546858] tun: Universal TUN/TAP device driver, 1.6
[ 2.552336] CAN device driver interface
[ 2.559032] pps pps0: new PPS source ptp0
[ 2.568434] libphy: fec_enet_mii_bus: probed
[ 2.574328] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.581281] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 2.587183] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 2.593215] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 2.600244] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 2.605914] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 2.613811] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 2.619828] sky2: driver version 1.30
[ 2.632404] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.638955] ehci-pci: EHCI PCI platform driver
[ 2.643501] ehci-platform: EHCI generic platform driver
[ 2.648976] ehci-exynos: EHCI EXYNOS driver
[ 2.653359] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.659565] ohci-pci: OHCI PCI platform driver
[ 2.664108] ohci-platform: OHCI generic platform driver
[ 2.669557] ohci-exynos: OHCI EXYNOS driver
[ 2.674448] Can't support > 32 bit dma.
[ 2.678339] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.683853] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 2.697878] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x01010810
[ 2.706645] xhci-hcd xhci-hcd.0.auto: irq 235, io mem 0x38200000
[ 2.713467] hub 1-0:1.0: USB hub found
[ 2.717257] hub 1-0:1.0: 1 port detected
[ 2.721609] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 2.727117] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 2.734849] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 2.742140] hub 2-0:1.0: USB hub found
[ 2.745979] hub 2-0:1.0: 1 port detected
[ 2.750862] usbcore: registered new interface driver usb-storage
[ 2.757039] usbcore: registered new interface driver usb_ehset_test
[ 2.766836] input: 30370000.snvs:snvs-powerkey as /devices/platform/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 2.780825] snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs-rtc-lp as rtc0
[ 2.790889] i2c /dev entries driver
[ 2.799368] ov5640_mipi 0-003c: No sensor reset pin available
[ 2.816423] ov5640_mipi 0-003c: Read reg error: reg=300a
[ 2.821805] ov5640_mipi 0-003c: Camera is not found
[ 2.826908] ov5640_mipi 1-003c: No sensor reset pin available
[ 2.844491] ov5640_mipi 1-003c: Read reg error: reg=300a
[ 2.849873] ov5640_mipi 1-003c: Camera is not found
[ 2.855704] mxc-mipi-csi2_yav 30a70000.mipi_csi1: mipi_csi2_probe
[ 2.861909] CSI: Registered sensor subdevice: mxc-mipi-csi2.0
[ 2.867739] mxc-mipi-csi2_yav 30a70000.mipi_csi: Remote device at /mipi_csi1@30a70000/port/endpoint1 XXX found
[ 2.877762] mxc-mipi-csi2_yav 30a70000.mipi_csi1: lanes: 2, name: mxc-mipi-csi2.0
[ 2.885593] mxc-mipi-csi2_yav 30b60000.mipi_csi2: mipi_csi2_probe
[ 2.891775] CSI: Registered sensor subdevice: mxc-mipi-csi2.1
[ 2.897545] mxc-mipi-csi2_yav 30b60000.mipi_csi: Remote device at /mipi_csi2@30b60000/port/endpoint1 XXX found
[ 2.907564] mxc-mipi-csi2_yav 30b60000.mipi_csi2: lanes: 2, name: mxc-mipi-csi2.1
[ 2.920377] imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)
[ 2.927357] Bluetooth: HCI UART driver ver 2.3
[ 2.931874] Bluetooth: HCI UART protocol H4 registered
[ 2.937025] Bluetooth: HCI UART protocol BCSP registered
[ 2.942402] Bluetooth: HCI UART protocol ATH3K registered
[ 2.947812] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.954392] Bluetooth: HCI UART protocol Broadcom registered
[ 2.960065] Bluetooth: HCI UART protocol QCA registered
[ 2.967114] sdhci: Secure Digital Host Controller Interface driver
[ 2.973311] sdhci: Copyright(c) Pierre Ossman
[ 2.978064] Synopsys Designware Multimedia Card Interface Driver
[ 2.985468] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.040700] mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA
[ 3.050907] sdhci-esdhc-imx 30b50000.usdhc: Got CD GPIO
[ 3.105897] mmc1: SDHCI controller on 30b50000.usdhc [30b50000.usdhc] using ADMA
[ 3.116752] update hantro voltage from 18446744073709551 mV to 1000 mV
[ 3.123559] hantrodec: module inserted. Major = 238
[ 3.130930] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.138104] caam 30900000.caam: ERA source: CCBVID.
[ 3.145920] caam 30900000.caam: device ID = 0x0a16040100000000 (Era 9)
[ 3.152471] caam 30900000.caam: job rings = 3, qi = 0, dpaa2 = no
[ 3.161823] caam_jr 30901000.jr0: Entropy delay = 3200
[ 3.167279] caam_jr 30901000.jr0: Entropy delay = 3600
[ 3.215085] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.240767] caam_jr 30901000.jr0: Instantiated RNG4 SH0.
[ 3.265228] mmc0: new HS400 MMC card at address 0001
[ 3.270872] mmcblk0: mmc0:0001 DG4016 14.7 GiB
[ 3.275784] mmcblk0boot0: mmc0:0001 DG4016 partition 1 4.00 MiB
[ 3.282078] mmcblk0boot1: mmc0:0001 DG4016 partition 2 4.00 MiB
[ 3.288392] mmcblk0rpmb: mmc0:0001 DG4016 partition 3 4.00 MiB
[ 3.300990] Alternate GPT is invalid, using primary GPT.
[ 3.306361] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 3.308438] caam_jr 30901000.jr0: Instantiated RNG4 SH1.
[ 3.338446] caam algorithms registered in /proc/crypto
[ 3.348962] caam_jr 30901000.jr0: registering rng-caam
[ 3.354588] caam 30900000.caam: caam pkc algorithms registered in /proc/crypto
[ 3.363322] platform caam_sm: blkkey_ex: 2 keystore units available
[ 3.369944] platform caam_sm: 64-bit clear key:
[ 3.373710] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.374317] mmcblk1: mmc1:aaaa SL16G 14.8 GiB
[ 3.376633] mmcblk1: p1 p2
[ 3.388521] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 3.394193] platform caam_sm: 64-bit black key:
[ 3.398793] platform caam_sm: [0000] 22 2c 9d cb d2 e4 13 e3
[ 3.404467] platform caam_sm: [0008] 01 a1 e5 8a ed f3 dd a8
[ 3.410193] platform caam_sm: 128-bit clear key:
[ 3.414825] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 3.420553] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 3.426225] platform caam_sm: 128-bit black key:
[ 3.430911] platform caam_sm: [0000] 4a 1f 40 ff dd 7c 00 2f
[ 3.436585] platform caam_sm: [0008] 7a 35 dc 43 4b 31 5d 41
[ 3.442257] platform caam_sm: 192-bit clear key:
[ 3.446889] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 3.452563] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 3.458237] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 3.463908] platform caam_sm: 192-bit black key:
[ 3.468539] platform caam_sm: [0000] 40 c3 25 36 4f 0e 72 61
[ 3.474213] platform caam_sm: [0008] 4e 2e 62 63 1c 03 29 e9
[ 3.479887] platform caam_sm: [0016] a3 1f 79 aa 22 29 cd 60
[ 3.485560] platform caam_sm: [0024] fa 9c 98 95 09 90 ac 76
[ 3.491231] platform caam_sm: 256-bit clear key:
[ 3.495863] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 3.501536] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 3.507209] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 3.512883] platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
[ 3.518554] platform caam_sm: 256-bit black key:
[ 3.523185] platform caam_sm: [0000] 69 4b ae 6f 96 2f 10 88
[ 3.528859] platform caam_sm: [0008] cb e6 6e 87 8b 08 67 9c
[ 3.534533] platform caam_sm: [0016] 32 25 03 89 8c 04 cc bb
[ 3.540206] platform caam_sm: [0024] 5b cf d7 d1 86 93 21 b0
[ 3.545876] platform caam_sm: 64-bit unwritten blob:
[ 3.550855] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 3.556529] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 3.562202] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 3.567875] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 3.573549] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 3.579222] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 3.584895] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 3.590568] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 3.596242] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.601915] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.607593] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.613267] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.618938] platform caam_sm: 128-bit unwritten blob:
[ 3.624004] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 3.629677] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 3.635350] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 3.641023] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 3.646696] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 3.652370] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 3.658044] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 3.663717] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 3.669390] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.675064] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.680737] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.686410] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.692082] platform caam_sm: 196-bit unwritten blob:
[ 3.697147] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 3.702821] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 3.708495] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 3.714169] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 3.719841] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 3.725514] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 3.731188] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 3.736861] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 3.742534] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.748207] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.753880] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.759554] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.765224] platform caam_sm: 256-bit unwritten blob:
[ 3.770289] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 3.775963] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 3.781637] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 3.787310] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 3.792983] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 3.798657] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 3.804331] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 3.810004] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 3.815677] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.821351] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.827023] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.832696] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.840781] platform caam_sm: 64-bit black key in blob:
[ 3.846025] platform caam_sm: [0000] 28 a0 5a 28 76 79 59 22
[ 3.851700] platform caam_sm: [0008] 52 dc 60 9b 8b a1 1d 9b
[ 3.857373] platform caam_sm: [0016] 58 0e 41 aa 2f 6c 87 46
[ 3.863052] platform caam_sm: [0024] 54 e5 cf 9d ab 80 df b6
[ 3.868726] platform caam_sm: [0032] eb e0 30 a4 16 e4 42 6c
[ 3.874400] platform caam_sm: [0040] b6 70 d5 73 90 e3 3b e4
[ 3.880074] platform caam_sm: [0048] 2d 60 26 9b 93 05 b8 f7
[ 3.885748] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 3.891421] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.897094] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.902767] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.908461] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.914133] platform caam_sm: 128-bit black key in blob:
[ 3.919460] platform caam_sm: [0000] 64 a3 91 e3 0b 9c 6a 09
[ 3.925134] platform caam_sm: [0008] b7 ed 9c f7 6d 08 e9 af
[ 3.930807] platform caam_sm: [0016] 57 6e 09 b0 c5 9c b6 9a
[ 3.936481] platform caam_sm: [0024] bd 32 fa 8f 02 a7 49 80
[ 3.942155] platform caam_sm: [0032] 57 ad 09 c7 f4 16 6f 0c
[ 3.947828] platform caam_sm: [0040] 0a 49 fe 26 fe 2f c1 7a
[ 3.953502] platform caam_sm: [0048] a9 fb 53 fd 31 79 6f 7e
[ 3.959175] platform caam_sm: [0056] e0 21 97 81 16 6c 76 1d
[ 3.964849] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 3.970529] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 3.976203] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 3.981876] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 3.987547] platform caam_sm: 192-bit black key in blob:
[ 3.992873] platform caam_sm: [0000] 13 c4 bf 89 ec 8a 96 2e
[ 3.998547] platform caam_sm: [0008] 4b b1 3b b6 be bd 54 97
[ 4.004221] platform caam_sm: [0016] ed 01 68 43 54 59 29 cc
[ 4.009894] platform caam_sm: [0024] b3 6f 4b 3c 50 5b 50 6e
[ 4.015567] platform caam_sm: [0032] 06 ae 37 b2 b0 68 5c d8
[ 4.021241] platform caam_sm: [0040] 50 96 18 10 22 13 b5 18
[ 4.026915] platform caam_sm: [0048] b4 f4 07 fd 05 01 9a 7f
[ 4.032588] platform caam_sm: [0056] 7b 32 3c d5 03 ca b3 04
[ 4.038261] platform caam_sm: [0064] 1a a9 47 84 46 eb 95 b1
[ 4.043934] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 4.049608] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 4.055281] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 4.060952] platform caam_sm: 256-bit black key in blob:
[ 4.066278] platform caam_sm: [0000] db 33 4d 03 29 20 6e 65
[ 4.071952] platform caam_sm: [0008] bd 8c 77 96 e3 05 ea 88
[ 4.077625] platform caam_sm: [0016] 82 a9 93 3f 95 f4 d3 1c
[ 4.083298] platform caam_sm: [0024] ea d4 62 02 d8 a6 ea 00
[ 4.088972] platform caam_sm: [0032] 73 df a5 79 ae ef 64 bc
[ 4.094646] platform caam_sm: [0040] a4 2c 74 4f 79 12 42 92
[ 4.100320] platform caam_sm: [0048] 30 34 40 21 dd 10 48 5c
[ 4.105994] platform caam_sm: [0056] 52 24 40 b2 b3 f5 68 70
[ 4.111668] platform caam_sm: [0064] 50 a7 4c 11 c8 7c 87 bd
[ 4.117345] platform caam_sm: [0072] 70 fa a1 7f a3 94 f3 49
[ 4.123019] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 4.128692] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 4.138595] platform caam_sm: restored 64-bit black key:
[ 4.143929] platform caam_sm: [0000] eb 03 c7 87 2c 11 48 04
[ 4.149604] platform caam_sm: [0008] fe fe e0 06 0a 86 bd 2a
[ 4.155276] platform caam_sm: restored 128-bit black key:
[ 4.160689] platform caam_sm: [0000] 4a 1f 40 ff dd 7c 00 2f
[ 4.166363] platform caam_sm: [0008] 7a 35 dc 43 4b 31 5d 41
[ 4.172034] platform caam_sm: restored 192-bit black key:
[ 4.177448] platform caam_sm: [0000] 40 c3 25 36 4f 0e 72 61
[ 4.183121] platform caam_sm: [0008] 4e 2e 62 63 1c 03 29 e9
[ 4.188795] platform caam_sm: [0016] c8 d1 89 12 ac 4f 1b 47
[ 4.194469] platform caam_sm: [0024] b7 62 e6 2c a5 c8 9f 04
[ 4.200144] platform caam_sm: restored 256-bit black key:
[ 4.205557] platform caam_sm: [0000] 69 4b ae 6f 96 2f 10 88
[ 4.211231] platform caam_sm: [0008] cb e6 6e 87 8b 08 67 9c
[ 4.216905] platform caam_sm: [0016] 32 25 03 89 8c 04 cc bb
[ 4.222578] platform caam_sm: [0024] 5b cf d7 d1 86 93 21 b0
[ 4.228716] caam-snvs 30370000.caam-snvs: can't get snvs clock
[ 4.234607] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state
[ 4.243072] usbcore: registered new interface driver usbhid
[ 4.248660] usbhid: USB HID core driver
[ 4.265019] random: fast init done
[ 4.269454] optee: probing for conduit method from DT.
[ 4.275041] optee: initialized driver
[ 4.307928] imx-wm8524 sound-wm8524: wm8524-hifi <-> 308b0000.sai mapping ok
[ 4.315006] imx-wm8524 sound-wm8524: ASoC: no DMI vendor name!
[ 4.326038] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 30810000.spdif mapping ok
[ 4.333692] imx-spdif sound-spdif: ASoC: no DMI vendor name!
[ 4.342734] imx-spdif sound-hdmi-arc: snd-soc-dummy-dai <-> 308a0000.spdif mapping ok
[ 4.350592] imx-spdif sound-hdmi-arc: ASoC: no DMI vendor name!
[ 4.363600] ak4458 2-0010: ASoC: failed to probe component -6
[ 4.369576] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6
[ 4.377038] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6)
[ 4.399695] ak5558 2-0013: ASoC: failed to probe component -6
[ 4.406096] imx-ak5558 sound-ak5558: ASoC: failed to instantiate card -6
[ 4.414490] imx-ak5558 sound-ak5558: snd_soc_register_card failed (-6)
[ 4.421449] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 4.428428] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 4.435661] NET: Registered protocol family 26
[ 4.440633] NET: Registered protocol family 10
[ 4.446087] Segment Routing with IPv6
[ 4.449861] NET: Registered protocol family 17
[ 4.454342] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 4.467362] can: controller area network core (rev 20170425 abi 9)
[ 4.473588] NET: Registered protocol family 29
[ 4.478100] can: raw protocol (rev 20170425)
[ 4.482382] can: broadcast manager protocol (rev 20170425 t)
[ 4.488111] can: netlink gateway (rev 20170425) max_hops=1
[ 4.494883] Bluetooth: RFCOMM TTY layer initialized
[ 4.499836] Bluetooth: RFCOMM socket layer initialized
[ 4.504996] Bluetooth: RFCOMM ver 1.11
[ 4.508815] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 4.514139] Bluetooth: BNEP filters: protocol multicast
[ 4.519432] Bluetooth: BNEP socket layer initialized
[ 4.524408] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 4.530395] Bluetooth: HIDP socket layer initialized
[ 4.535408] lib80211: common routines for IEEE802.11 drivers
[ 4.541169] 9pnet: Installing 9P2000 support
[ 4.545544] Key type dns_resolver registered
[ 4.551542] registered taskstats version 1
[ 4.564496] hantro receive hot notification event: 0
[ 4.569491] cpu cpu0: registered imx8mq-cpufreq
[ 4.575124] OF: PCI: host bridge /pcie@0x33800000 ranges:
[ 4.580538] OF: PCI: No bus range found for /pcie@0x33800000, using [bus 00-ff]
[ 4.588146] OF: PCI: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 4.594077] OF: PCI: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 4.600427] imx6q-pcie 33800000.pcie: pcie phy pll is locked.
[ 4.679562] imx6q-pcie 33800000.pcie: Speed change timeout
[ 4.685055] imx6q-pcie 33800000.pcie: Roll back to GEN1 link!
[ 4.690809] imx6q-pcie 33800000.pcie: Link up, Gen1
[ 4.697243] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00
[ 4.703612] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 4.709160] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 4.715348] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff]
[ 4.732277] pci 0000:00:00.0: BAR 14: assigned [mem 0x18000000-0x185fffff]
[ 4.739227] pci 0000:00:00.0: BAR 0: assigned [mem 0x18600000-0x186fffff 64bit]
[ 4.746612] pci 0000:00:00.0: BAR 6: assigned [mem 0x18700000-0x1870ffff pref]
[ 4.753908] pci 0000:01:00.0: BAR 2: assigned [mem 0x18000000-0x183fffff 64bit]
[ 4.761271] pci 0000:01:00.0: BAR 0: assigned [mem 0x18400000-0x18407fff 64bit]
[ 4.768687] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 4.773929] pci 0000:00:00.0: bridge window [mem 0x18000000-0x185fffff]
[ 4.781232] pcieport 0000:00:00.0: Signaling PME with IRQ 240
[ 4.787151] pcieport 0000:00:00.0: AER enabled with IRQ 240
[ 4.793794] OF: PCI: host bridge /pcie@0x33c00000 ranges:
[ 4.799213] OF: PCI: No bus range found for /pcie@0x33c00000, using [bus 00-ff]
[ 4.806772] OF: PCI: IO 0x27f80000..0x27f8ffff -> 0x00000000
[ 4.812712] OF: PCI: MEM 0x20000000..0x27efffff -> 0x20000000
[ 4.819236] imx6q-pcie 33c00000.pcie: pcie phy pll is locked.
[ 5.069122] imx6q-pcie 33c00000.pcie: phy link never came up
[ 5.074807] imx6q-pcie 33c00000.pcie: failed to initialize host
[ 5.080739] imx6q-pcie 33c00000.pcie: unable to add pcie port.
[ 5.086622] imx6q-pcie: probe of 33c00000.pcie failed with error -110
[ 5.097208] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 5.104190] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 5.112414] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
[ 5.122289] ALSA device list:
[ 5.125274] #0: wm8524-audio
[ 5.128391] #1: imx-spdif
[ 5.131186] #2: imx-hdmi-arc
[ 5.159276] EXT4-fs (mmcblk1p2): recovery complete
[ 5.165750] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 5.173895] VFS: Mounted root (ext4 filesystem) on device 179:130.
[ 5.185369] devtmpfs: mounted
[ 5.188676] Freeing unused kernel memory: 1280K
[ 5.319998] systemd[1]: System time before build time, advancing clock.
[ 5.333741] systemd[1]: systemd 237 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 5.355401] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 4.14-sumo (sumo)!

[ 5.396444] systemd[1]: Set hostname to <imx8mqevk>.
[ 5.475933] systemd[1]: File /lib/systemd/system/systemd-journald.service:35 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 5.493064] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 5.584221] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.591146] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 5.616438] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.623148] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 5.640386] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.648303] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.668234] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.688500] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Created slice System Slice.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Created slice system-getty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Listening on udev Kernel Socket.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Syslog Socket.
[ OK ] Reached target Slices.
[ OK ] Listening on Journal Socket.
Mounting Kernel Debug File System...
Mounting POSIX Message Queue File System...
Starting Apply Kernel Variables...
Starting Journal Service...
Mounting Huge Pages File System...
Starting udev Coldplug all Devices...
Mounting Temporary Directory (/tmp)...
Mounting Kernel Configuration File System...
[ OK ] Started feed random number from /dev/hwrng to /dev/random.
[ OK ] Reached target Paths.
Starting Remount Root an[ 6.073655] random: crng init done
d Kernel File Systems...
[ 6.077375] random: 7 urandom warning(s) missed due to ratelimiting
[ 6.080366] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Remount Root and Kernel File Systems.
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Create Static Device Nodes in /dev.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
[ OK ] Reached target Containers.
Mounting /var/volatile...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /var/volatile.
[ 6.401512] systemd-journald[1931]: Received request to flush runtime journal from PID 1
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Network Service...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Load/Save Random Seed.
Starting Create Volatile Files and Directories...
[ OK ] Started Network Service.
[ OK ] Started Create Volatile Files and Directories.
[ OK ] Found device /[ 6.532435] imx-sdma 302c0000.sdma: external firmware not found, using ROM firmware
dev/ttymxc0.
[ 6.543061] imx-sdma 30bd0000.sdma: external firmware not found, using ROM firmware
Starting Network Time Synchroniz[ 6.567675] wlan_cnss_core_pcie: loading out-of-tree module taints kernel.
ation...
[ 6.583121] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 6.591474] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 6.598885] msm_ipc_router_init-Enter-
[ 6.603890] NET: Registered protocol family 27
[ 6.608608] msm_ipc_router_init-Exit-
[ 6.613135] ipc_router_mhi_xprt_probe--Enter--
[ 6.618128] ipc_router_mhi_xprt_probe--Exit--
[ 6.625019] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 6.633128] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
Starting Update UTMP about System[ 6.633545] cnss: bus type selected 0
Boot/Shutdown...
[ 6.633660] cnss: created sysfs for vreg-wlan-en control
[ 6.633899] cnss: Platform driver probed successfully.
[ 6.634108] diagchar initializing ..
[ 6.634112] diagchar initialized now
[ 6.634323] diag_mhi_probe start
[ 6.634693] diag: mhi device is ready
[ 6.676965] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 6.684096] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
Starting Network Name Resolution...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Network.
[ OK ] Reached target Sound Card.
[ OK ] Reached target System Time Synchronized.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started TEE Supplicant.
Starting Login Service...
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Started Kernel Logging Service.
Starting Permit User Sessions...
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Login Service.
[ OK ] Started Permit User Sessions.
[ OK ] Started Serial Getty on ttymxc0.
[ OK ] Started Getty on tty1.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.

NXP i.MX Release Distro 4.14-sumo imx8mqevk ttymxc0

imx8mqevk login: root (automatic login)

[ 7.485485] audit: type=1006 audit(1619179443.743:2): pid=3206 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
root@imx8mqevk:~#
root@imx8mqevk:~#
root@imx8mqevk:~#
root@imx8mqevk:~#
root@imx8mqevk:~#
root@imx8mqevk:~# lspci -vv
00:00.0 PCI bridge: Synopsys, Inc. Device abcd (rev 01) (prog-if 00 [Normal decode])
Control: I/O+ Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR+ FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Latency: 0
Interrupt: pin A routed to IRQ 240
Region 0: Memory at 18600000 (64-bit, non-prefetchable) [size=1M]
Bus: primary=00, secondary=01, subordinate=ff, sec-latency=0
I/O behind bridge: None
Memory behind bridge: 18000000-185fffff [size=6M]
Prefetchable memory behind bridge: None
Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
[virtual] Expansion ROM at 18700000 [disabled] [size=64K]
BridgeCtl: Parity- SERR- NoISA- VGA- MAbort- >Reset- FastB2B-
PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1+ D2- AuxCurrent=375mA PME(D0+,D1+,D2-,D3hot+,D3cold+)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [50] MSI: Enable+ Count=1/1 Maskable+ 64bit+
Address: 000000004415a000 Data: 0000
Masking: 00000000 Pending: 00000000
Capabilities: [70] Express (v2) Root Port (Slot-), MSI 00
DevCap: MaxPayload 128 bytes, PhantFunc 0
ExtTag- RBE+
DevCtl: Report errors: Correctable+ Non-Fatal+ Fatal+ Unsupported+
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop-
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 5GT/s, Width x1, ASPM L0s L1, Exit Latency L0s <1us, L1 <64us
ClockPM- Surprise- LLActRep+ BwNot+ ASPMOptComp+
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk+
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive+ BWMgmt+ ABWMgmt-
RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna+ CRSVisible-
RootCap: CRSVisible-
RootSta: PME ReqID 0000, PMEStatus- PMEPending-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR-, OBFF Not Supported ARIFwd-
AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled ARIFwd-
AtomicOpsCtl: ReqEn- EgressBlck-
LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
Capabilities: [100 v2] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
HeaderLog: 00000000 00000000 00000000 00000000
RootCmd: CERptEn+ NFERptEn+ FERptEn+
RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
Capabilities: [148 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2- ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=10us PortTPowerOnTime=10us
L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
T_CommonMode=10us
L1SubCtl2: T_PwrOn=10us
Kernel driver in use: pcieport

01:00.0 Network controller: Broadcom Limited BCM4356 802.11ac Wireless Network Adapter (rev 02)
Subsystem: Broadcom Limited BCM4356 802.11ac Wireless Network Adapter
Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx-
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Interrupt: pin A routed to IRQ 0
Region 0: Memory at 18400000 (64-bit, non-prefetchable) [disabled] [size=32K]
Region 2: Memory at 18000000 (64-bit, non-prefetchable) [disabled] [size=4M]
Capabilities: [48] Power Management version 3
Flags: PMEClk- DSI- D1+ D2+ AuxCurrent=0mA PME(D0+,D1+,D2+,D3hot+,D3cold+)
Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=2 PME-
Capabilities: [58] MSI: Enable- Count=1/16 Maskable- 64bit+
Address: 0000000000000000 Data: 0000
Capabilities: [68] Vendor Specific Information: Len=44 <?>
Capabilities: [ac] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <4us, L1 unlimited
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset- SlotPowerLimit 0.000W
DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
RlxdOrd+ ExtTag- PhantFunc- AuxPwr+ NoSnoop+
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr+ TransPend-
LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s L1, Exit Latency L0s <2us, L1 <32us
ClockPM+ Surprise- LLActRep- BwNot- ASPMOptComp+
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk+
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, LTR+, OBFF Via WAKE#
AtomicOpsCap: 32bit- 64bit- 128bitCAS-
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
AtomicOpsCtl: ReqEn-
LnkCtl2: Target Link Speed: 2.5GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -3.5dB, EqualizationComplete-, EqualizationPhase1-
EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
Capabilities: [100 v1] Advanced Error Reporting
UESta: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UEMsk: DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
CESta: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr-
CEMsk: RxErr- BadTLP- BadDLLP- Rollover- Timeout- NonFatalErr+
AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
HeaderLog: 00000000 00000000 00000000 00000000
Capabilities: [13c v1] Device Serial Number 00-00-38-ff-ff-00-38-0f
Capabilities: [150 v1] Power Budgeting <?>
Capabilities: [160 v1] Virtual Channel
Caps: LPEVC=0 RefClk=100ns PATEntryBits=1
Arb: Fixed- WRR32- WRR64- WRR128-
Ctrl: ArbSelect=Fixed
Status: InProgress-
VC0: Caps: PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
Arb: Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
Ctrl: Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
Status: NegoPending- InProgress-
Capabilities: [1b0 v1] Latency Tolerance Reporting
Max snoop latency: 0ns
Max no snoop latency: 0ns
Capabilities: [220 v1] #15
Capabilities: [240 v1] L1 PM Substates
L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
PortCommonModeRestoreTime=0us PortTPowerOnTime=50us
L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
T_CommonMode=0us LTR1.2_Threshold=0ns
L1SubCtl2: T_PwrOn=10us

0 项奖励
回复
1 回复

1,101 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Lim

 

one can try to disable it in dts, change "&pcie" status to disabled

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk.d...

 

Best regards
igor

0 项奖励
回复