Hi everyone,
I successfully run the echo example on my custom board based on i.MX 8M Mini.
imx_rpmsg_tty module works and I'm able to send some bytes from A53 to M4.
The example anyway should write back the same bytes via the rpmsg_lite_send_nocopy function from M4 to A53.
In fact I find these line with dmesg
[ 3.572174] rpmsg_tty_cb68 65 6c 6c 6f 20 77 6f 72 6c 64 21 hello world!
but if i run this command:
cat /dev/ttyRPMSG
the output is empty.
Of course i can run
echo blabla > /dev/ttyRPMSG
and just like before I find the answer from M4 with dmesg but the cat command gives an empty result.
What's the correct procedure to read the tty?
Thank you!
解決済! 解決策の投稿を見る。
you need to assigns it a file descriptor, writes and reads to int, then closes it, pls refer to the "step 5"
you need to assigns it a file descriptor, writes and reads to int, then closes it, pls refer to the "step 5"