已解决! 转到解答。
1. evkbimxrt1050_flexspi_nor_config.c is suitable for the hyperflash S26KS512 on rt1170
2. It should be MIMXRT1170_UFL_L2 for the hyperflash S26KS512
You can set boot mode to 2'b01 - SDP mode, then try again.
Are you following below two blogs to use UFL?
超级下载算法RT-UFL v1.0发布,附J-Link下安装教程
超级下载算法RT-UFL v1.0在MCUXpresso IDE下的使用
What is the FlexSPI pin connection to S26KS512 in your board?
Hi @jay_heng,
Do you have any idea about my recent reply? Or can you help provide the right hyperflash configration of S26KS512 in rt1170 XIP and the sutiable .cfx file for S26KS512 of rt1170?
Thanks.
Hi @jay_heng,
Thanks for support.
The FlexSPI pin connection to S26KS512 on my board is like the following picture shows.
pin
I followed your blogs to use UFL, just like the discription I mentioned before, I also tried Jlink download but failed, and when I tried to read back the flash, it also failed. The result is like the following.
download_error
read_back_error
I think the problem may come from the complied bin or the hyperflash driver, can you help check the following questions?
1. Is the configuration in evkbimxrt1050_flexspi_nor_config.c suitable for the hyperflash S26KS512 on rt1170?
2. Can the driver MIMXRT1170_UFL_L1/L2 work normally for the hyperflash S26KS512 on rt1170?
3. Is there any configuration I omit?
Thanks.
1. evkbimxrt1050_flexspi_nor_config.c is suitable for the hyperflash S26KS512 on rt1170
2. It should be MIMXRT1170_UFL_L2 for the hyperflash S26KS512
You can set boot mode to 2'b01 - SDP mode, then try again.
Hi @jay_heng
I have a question that whether setting boot mode to 2'b01 and programing flash with JLink is exact SDP mode, or setting boot mode to 2'b01 and programing flash with UART/USB is just exact SDP mode, as I notice this discription in "i.MX RT1170 Processor Reference Manual".
What's more, my board enter an error state that even ram can't be programed, and I guess it is because of some wrong flash programing tests. How can I make the board restore to the initial state that I can program the ram for debug at least before I can program the flash normally? It's important to point out that I don't have UART/USB to enter SDP mode, and I just have JLink now. So is there any software or hardware method to restore it?
Thanks.
Hi @yalin ,
Thanks for your reply.
Can the Jlink be able to detect the core in Jlink commander either the BOOT_MODE[1:0]= 01 or other settings?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @jeremyzhou
Thanks for support.
Actually Jlink can be able to connect. And with Jlink, I can program the ram when setting boot mode to 2'b01 now, but can't program the ram in internal boot mode, I think this may be because of some wrong flash programing tests. And I can't program the flash still in either 2'b01 or internal boot mode just with Jlink.
So in my situation, without UART or USB,
1.Is there any way to restore my board to the initial state that I can program the ram in internal boot mode?
2.Is there other way to program my flash just with Jlink beside the ways mentioned before?
Thanks.
Hi,
I'd like to suggest two ways to recover, the first way is trying to trigger the enter debug action after setting boot mode to 2'b01, for instance, debug a hello_world demo, etc.
Next, you can try to load a demo code in the ram when setting boot mode to 2'b01, and the demo code should be able to erase the blocks of hyperflash S26KS512.
Please give it a try.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @jeremyzhou
As I know that triggering the debug action when setting boot mode to 2'b01 with UART can restore the board from a flash error state, should this method be effective with Jlink theoretically?
I'm sorry but I have tried the two methods you mentioned when setting boot mode to 2'b01 with Jlink, after that I can't program the ram in internal boot mode also.
Can you help check that?
Thanks.
Hi @yalin ,
Thanks for your reply.
Please refer to the attached demo, then try to load a demo code into RAM to run for erasing S26KS512.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for your support.
I have a test board with uart now and try to flash it with MCU Boot Utility, but it failed when click "configure boot device" as the picture shows.
configure boot device error
The boot device configuration is like the following.
boot device configuration
And I switch the BOOT_CFG[9] to ON according to the following discription in MIMXRT1170-EVK schematic.
boot_cfg
So is the boot_cfg right for hyperflash? Or is there any hardware signal to check?
Thanks.
Hi,
Thanks for your reply.
Firstly, I was wondering if you can share the schematic of this board,
next, please use the
evkbimxrt1050_flexspi_hyper_flash_polling_transfer demo to try to access the Hyperflash,
lastly, can you upload the log of the MCU Boot Utility.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------