How to place iMX8DXL into KS0 low power mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to place iMX8DXL into KS0 low power mode

618件の閲覧回数
chirag_patel1
Contributor I

Does iMX8DXL automatically enter KS0 mode if only VDD_SNVS_4P2 pin is powered by 3.3V and 32kHz external crystal across RTC_XTALI/XTALO pins? If not, how do you enable KS0 low power mode?

What is the current draw in this mode when external 32kHz crystal is present versus external crystal not present?

0 件の賞賛
返信
1 返信

582件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chirags

you are right, power consumption details can be found in sect.4.1.1.

KS0 – SNVS-Only mode AN12338

i.MX 8QuadXPlus Power Consumption Measurement

sect.4.1.6 Low power mode supply currents

i.MX 8DualX Automotive and Infotainment Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信