How to pass DMA buffers from a Driver thru GStreamer 'v4l2src' plugin to Freescale IPU/VPU plugins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to pass DMA buffers from a Driver thru GStreamer 'v4l2src' plugin to Freescale IPU/VPU plugins

32,405 Views
ilkodossev
Contributor III

Intro

Most of the hardware nowadays is capable of doing DMA transfers on large amount of data. Noticeably, Camera Capture Drivers (or any driver which delivers data to from any outside source to memory) can request DMA-capable buffer and put data into it.

While V4L2 architecture allows any driver to configure its DMA memory usage, it does not facilitate export of such information to Clients. Speccifically, GStreamer plugin implementation suffers terribly from the need to do incredible amount of byte-pushing in User Space, in order to pass buffer data from plugin to plugin. The incurred performance penalty is enormous!

The implementation I worked on involved TW6869 Camera capture chip which is DMA-capable; the captured RGB (or YUV) buffer had to be converted and compressed before further processing. Naturally, IPU mirroring capabilities and VPU compression capabilities determined the pipeline configuration. Also as natural pipeline builder came GST, together with its performance penalty mentioned above.

Hence, the goal becomes to connect "v4l2src" plugin with FSL plugins in a manner which allows recognition and use of DMA buffers, thus avoiding memcpy of data altogether.

Freescale's plugins do employ internal architecture of passing DMABLE info to each other, but in addition to this internal architecture, these plugins do use a more universal method to detect a DMA address.

These methods employed by Freescale plugins require patches in both "Video4Linux2" subsystem and in GStreamer's "libgstvideo4linux2.so" library.

Credit is due to Peng Zhou from Freescale for providing me with to-the-point information regarding Freescale's DMA implementation.

V4L2 patch

V4L2 uses "v4l2_buffer" structure (videodev2.h) to communicate with its clients. This structure, however, does not natively indicate to the Client whether the buffer just captured has DMA address.

Two members in the structure need attention:

     __u32     flags;

     __u32     reserved;

For "flags" a new flag hasto be defined:

  #define V4L2_BUF_FLAG_DMABLE    0x40000000  /* buffer is DMA-mapped, 'reserved' contains DMA phy address */

And, accordingly, the Driver has to set the flag and fill in the "reserved" member in both its "vidioc_querybuf" and "vidioc_dqbuf" implementations.

This done, all V4L2 clients will get the DMA information from the Driver, for each of its buffers.

GST plugin patch

This patch is more difficult to implement. Not just acquisition of a DMA address from V4L2 driver is necessary, but then passing along that information to the next plugin in the pipeline is a must.

Plugins communicate with each other using "GstBuffer" structure, which like its V4L2 cousin has no provisions for passing DMA information.

Naturally, in a pipeline where FSL plugins are involved, a FSL-compatible method should be implemented. These are the macros used in FSL plugins:

  #define IS_DMABLE_BUFFER(buffer)

  #define DMABLE_BUFFER_PHY_ADDR(buffer)

The most FSL-compatible way to implement DMABLE would be to use "_gst_reserved" extension in the structure. If maximum compatibility with FSL is the goal, then a closer look at "gstbufmeta.c" and "gstbufmeta.h" files in "gst-fsl-plugins-3.0.7/libs/gstbufmeta/" folder shall be taken. Alternatively, GST_BUFFER_FLAG_LAST and GST_BUFFER_OFFSET may be used.

The sources of GStreamer's "libgstvideo4linux2.so" need patches in several places. First of all, right after calls to VIDIOC_QUERYBUF and VIDIOC_DQBUF the information from "v4l2_buffer" must be put in the "GstBuffer" instance. Next, the "need_copy" and "always_copy" flags have to be overridden whenever GST_BUFFER_FLAG_LAST is set. For reasons I cannot explain, the macro PROP_DEF_ALWAYS_COPY in the GST sources is set to TRUE and it is the default for "always_copy"! The final -- and absolutely important patch, is to prevent overwriting of GST_BUFFER_OFFSET memeber with sequential buffer number. Very! Bad! Things! will happen to the system if improper value is passed along as physical address! This last fix can be made conditional, upon the presence of GST_BUFFER_FLAG_LAST.

The outcome

Once these patches are in place, the pipeline is ready to roll, ansd roll it will really fast! My measurements by injection timing traces in FSL's "vpuenc" plugin demonstrated that the time for acquisition of GST input buffer was reduced on the average from 3+ milliseconds to 3-5 microseconds; and this improvement does not include the savings from avoiding the copy inside "libgstvideo4linux2.so" caused by "always_copy" flag!

Universally DMABLE?

The most important conclusion/question from the implementation above ought to be:
"Isn't it time for both V4L2 and GST to enable DMA buffer recognition and physical pointer passing?"

It is my firm belief, that such feature will result in great performance improvements for all kinds of video/audio streaming.

Ilko Dossev

Qualnetics, Inc.

Labels (2)
43 Replies

13,022 Views
draven
Contributor III

Hi @Sasamy ,

 I could work with kernel 4.19 on imx8qxp your driver for get tw6869 channels via dma.

But I built for imx8qxp with kernel 5.4 but video channels did not appear and error register  videos. Is there any version for kernel 5.4 or What I have to change for kernel 5.4?

 

0 Kudos
Reply

13,910 Views
leonardoveiga
Contributor I

Hello everyone,

I am trying to use the tw68 driver with the tw6816. I tried many pipelines already and the last I am trying is:

gst-launch-1.0 --gst-debug-level=3 imxv4l2videosrc input=0 ! imxipuvideosink use-vsync=true

I have added debug print to the functions of the tw68-video.c, and it seems that the device is working (it detects when there is no video input connected, get video standard, etc). It also seems that the DMA is being configured - it is setting 3 buffers for DMA.

When I run the gstreamer pipeline above, there is only a black screen. When I tried a filesink instead of imxipuvideosink, the file always have 0 bytes. It seems that gstreamer is getting no data from the tw6816.

Does anyone have any tips regarding DMA debug? I read in the original question "And, accordingly, the Driver has to set the flag and fill in the "reserved" member in both its "vidioc_querybuf" and "vidioc_dqbuf" implementations." but have no idea how do I know what DMA address to pass to "reserved", for instance.

Any tips are appreciated.

Best regards,

Leonardo

0 Kudos
Reply

13,907 Views
tengri
Contributor IV

Doesn't disabling pci msi in kernel help you at all ? passing pci=nomsi in kernel command line should work if there is no problem in your hardware and memory allocation.

0 Kudos
Reply

13,910 Views
fabiendelafonta
Contributor I

Hi,

I try also to capture and encode 8 D1 videos from tw6869 at 25ips.

What's the driver you are using for the tw6869? Have you modify the driver for he send dma address?

I tried to modify the mfw_v4L2src plugin for work with the tw6869, but gstreamer crash in "mfw_gst_ipu_core_start_convert" (in mfw_gst_ipu_csc.c) because the dma address is NULL.

Have you made a patch for v4l2src plugin and the driver ?

Thanks advance.

Fabien

0 Kudos
Reply

13,927 Views
varsmolta
Contributor V

Nice work! is there a patch for this? Any plans or rolling this into the freescale gstreamer and kernel repositories?

0 Kudos
Reply

13,927 Views
ilkodossev
Contributor III

The only patch really necessary is for GST v4l2src plugin.

It will be posted shortly, right after I am done with my current & very urgent project. :smileyhappy:

Regarding "videodev2.h" -- it also needs the definition, but for now a workaround like this will be sufficient in any source file:

#ifndef V4L2_BUF_FLAG_DMABLE

#define V4L2_BUF_FLAG_DMABLE        0x40000000

#endif

0 Kudos
Reply

13,910 Views
varunchaudhary
Contributor I

Hi Ilko Dossev,

As you said, that we've to pass DMAble information from pcie capture card  through v4l2 to its clients. I am using ffmpeg for encode/decode purpose.I am keen to know that , as you mentioned in one of your posts

----------------------------------------------------------------------------------------------------------------------------------------------------------------

This is currently working implementation:
CamCap => [RGB DMA buffer] => IPU => [YUV420 DMA buffer] => GStreamer => [YUV420 DMA buffer] => VPU => [AVC DMA buffer] => GStreamer => final sink

To my greatest chagrin, GStreamer operations involve a lot of memcpy from and to DMA buffers, which is performance killer.

A useful practical implementation would be this:
CamCap => [RGB DMA buffer] => IPU => [YUV420 DMA buffer] => VPU => [AVC DMA buffer] => GStreamer => final sink

Feeding directly IPU output to VPU input would save a ton of memcpy operations; leaving one only at the end when compressed data are passed to GStreamer.

Ideal dream-stream would be setting up IPU and VPU to work in sequence, passing data internally:
CamCap => [RGB DMA buffer] => IPU => [...] => VPU => [AVC DMA buffer] => GStreamer => final sink

There is one catch here, though -- because the time for processing a frame is about 2.5 milliseconds, the combined IPU/VPU team should deliver within this limit!

(A total of 360 FPS for the whole system leaves less than 3 milliseconds processing time for each processing step.)

I moved a lot of source code from "libvpu" library to my Kernel Driver, and I am able to initialize VPU properly from my KO.

-------------------------------------------------------------------------------------------------------------------------------------------------------------------

1. Do we need someone in between IPU <==> V4l2 to read those pcie captured frames and feed them to IPU , as currently there is only parallel and mipi camera interface is supported in i.mx6 soc.

2. Does it require to move sources from libvpu to kernel space , to make the pt no. 1 to work properly.

Regards,

Varun

0 Kudos
Reply

13,927 Views
timharvey
Contributor IV

Ilko,


I have users asking about using TW6869 with IMX6 as well. Will you share your patches with the community?


Regards,


Tim

0 Kudos
Reply

13,927 Views
Sasamy
Contributor IV

Hi Tim,

we are currently working on a prototype boards based on tw6869, driver uses  vb2 api, but is also compatible with freescale gst-fsl-plugins through a small transparent hack.

In the Linux kernel driver:

+static int buffer_init(struct vb2_buffer *vb)

+{

+    struct tw6869_vbuffer *vbuf = to_tw6869_vbuffer(vb);

+

+    vbuf->dma = vb2_dma_contig_plane_dma_addr(vb, 0);

+    INIT_LIST_HEAD(&vbuf->list);

+    {    /* this hack to make gst-fsl-plugins happy */

+        u32 *cpu = vb2_plane_vaddr(vb, 0);

+        *cpu = vbuf->dma;

+    }

+    return 0;

+}

in tvsrc plugin:

@@ -220,22 +221,19 @@ mfw_gst_tvsrc_start_capturing (MFWGstTVS

         GST_BUFFER_SIZE (v4l_src->buffers[i]),

         PROT_READ | PROT_WRITE, MAP_SHARED,

         v4l_src->fd_v4l, GST_BUFFER_OFFSET (v4l_src->buffers[i]));

-    memset (GST_BUFFER_DATA (v4l_src->buffers[i]), 0xFF,

-        GST_BUFFER_SIZE (v4l_src->buffers[i]));

     {

       gint index;

       GstBufferMeta *meta;

       index = G_N_ELEMENTS (v4l_src->buffers[i]->_gst_reserved) - 1;

       meta = gst_buffer_meta_new ();

-      meta->physical_data = (gpointer) (buf->m.offset);

+      meta->physical_data =

+            (gpointer)(*(unsigned int *)(GST_BUFFER_DATA (v4l_src->buffers[i])));

       v4l_src->buffers[i]->_gst_reserved[index] = meta;

     }

+    memset (GST_BUFFER_DATA (v4l_src->buffers[i]), 0xFF,

+        GST_BUFFER_SIZE (v4l_src->buffers[i]));

the current version of the patch and test scripts in an attachment,

known Issues:

1 synchronization of audio and video in the encoding pipeline (probably a bug in the alsasrc plugin in gst 0.10)

2 sometimes, encoding pipeline is stalled for a considerable time (0.5 - 1 second)

Alexander

13,926 Views
timharvey
Contributor IV

Alexander,


This is great - thank you very much for sharing your work.

Have you ever looked into using the IMX6 hardware (IPU/VPU/GPU) to composite multiple streams into one so as to efficiently take the 4 (or more) streams into a single stream prior to sending to vpuenc? I have a user asking specifically for this.

Regards,

Tim

0 Kudos
Reply

13,930 Views
Sasamy
Contributor IV

Hi Tim,

I think this is not necessary because VPU "can encode or decode multiple video clips with multiple standards simultaneously", but some frames are discarded even in one simple pipeline, so i think real problem - slow color space conversion (UYVY -> I420 or NV12 that required for VPU) and/or bugs in software. in any case, we have no plans to deep dive in these issues.

Alexander.

0 Kudos
Reply

13,930 Views
timharvey
Contributor IV

Alexander,

Right - the VPU 'can' encode multiple streams simultaneously but what I'm interested in is combining multiple sources into a single stream (think videobox) before encoding it to a single stream. I haven't had time to integrate your patches yet to see if an IMX6DL or IMX6Q has enough CPU to combine 4x of these sources via a non VPU-enhanced videobox and keep up with 30fps. I also want to take a look at the gstreamer-imx plugins for gstreamer1.x. I don't see any documentation o them but it looks like there are a lot more options available.

Regards,

Tim

0 Kudos
Reply

13,928 Views
Sasamy
Contributor IV

Hi Tim,

I think blit that uses CPU  (videobox + videomix) is very inefficient on embedded processors.  gstreamer-imx have very good plugins that use gal2d, for example, on i.MX 6Solo and 6 streams I did not see the frame dropping with imxg2dvideosink, unfortunately gal2d has important limitations "RGB and YUV formats can be set in source surface, but only RGB format can be set in destination surface"

imx6_solo.png

Alexander

0 Kudos
Reply

13,928 Views
Sasamy
Contributor IV

Hello,

in an attachment - a stable version of the driver.

Alexander

13,909 Views
Sasamy
Contributor IV

Hello, in attachment the new version of the driver:

1 for gstreamer-imx plugins (master branch) patch/hack isn't required any more

https://github.com/Freescale/gstreamer-imx

2 MSI support should be disabled in the kernel config

Screenshot from 2015-07-03 10_03_07.png

Screenshot from 2015-07-03 10_03_21.png

3 for FSL Linux kernels 3.14.xx requires a patch to support the legacy interrupts

https://community.freescale.com/thread/353000

https://dev.openwrt.org/browser/trunk/target/linux/imx6/patches-3.14?rev=41004&order=name

0055-ARM_dts_imx_fix-invallid-#address-cells-value.patch

4 theoretically, driver should work with any kernels 3.10+

Alexander

13,909 Views
svens
Contributor I

Hi,

I've added an alias to the driver so it automatically loads once connected to the PCI bus. Just added this to the bottom of the file.

MODULE_ALIAS("pci:v*00001797d00006869sv*sd*bc*sc*i*");

Sven

0 Kudos
Reply

13,910 Views
Sasamy
Contributor IV

Hi Sven,

the kernel provides the macro MODULE_DEVICE_TABLE for generation of such information

static const struct pci_device_id tw6869_pci_tbl[] = {

    {PCI_DEVICE(PCI_VENDOR_ID_TECHWELL, PCI_DEVICE_ID_6869)},

    {PCI_DEVICE(PCI_VENDOR_ID_TECHWELL, PCI_DEVICE_ID_6865)},

    { 0, }

};

MODULE_DEVICE_TABLE(pci, tw6869_pci_tbl);

I forgot about it. Thanks.

Alexander

0 Kudos
Reply

13,910 Views
Sasamy
Contributor IV

Hello,

in an attachment the new stable version of the driver and some test scripts for gstreamer-imx

Alexander

13,910 Views
psidhu
Contributor III

Hi Alexander,

Thanks for all your work on this. I'm curious, where are you getting these new drivers? Is there a git tree somewhere that we can view?

- Pushpal

0 Kudos
Reply

13,910 Views
Sasamy
Contributor IV

Hi Pushpal Sidhu,

I created the project on GitHub

sasamy/tw6869 · GitHub

Alexander