How to migrate form i.MX8QXP to i.MX8DX ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to migrate form i.MX8QXP to i.MX8DX ?

Jump to solution
735 Views
mamorukanou
Contributor IV

We currently developing a board with (i.MX8QXP + DDR3L16bit) and running Linux (L4.14.98_2.0.0).

We plan to replace i.MX8QXP with i.MX8DX in the future, so we are starting software porting for i.MX8DX.

The following content is recognized as a change point from i.MX8QXP to i.MX8DX.

1) u-boot: Change USB3.0 to USB2.0
CONFIG_USB_XHCI_HCD = n
CONFIG_USB_XHCI_IMX8 = n

2) device tree: GPU Clock down
& gpu_3d0 {
-assigned-clock-rates = <700000000>, <850000000>;
+ assigned-clock-rates = <372000000>, <372000000>;

Besides this, Ether is also changed to 1G-> 100M. Do we need to modify the device tree for this?

If so, how should it be corrected?

If there are other points that need to be corrected, please let me know.

BR,

Kanou

0 Kudos
1 Solution
619 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Could you please submit a case?

There is some information that could not be shown here.

Best regards,

Diego.

View solution in original post

0 Kudos
1 Reply
620 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Could you please submit a case?

There is some information that could not be shown here.

Best regards,

Diego.

0 Kudos