We currently developing a board with (i.MX8QXP + DDR3L16bit) and running Linux (L4.14.98_2.0.0).
We plan to replace i.MX8QXP with i.MX8DX in the future, so we are starting software porting for i.MX8DX.
The following content is recognized as a change point from i.MX8QXP to i.MX8DX.
1) u-boot: Change USB3.0 to USB2.0
CONFIG_USB_XHCI_HCD = n
CONFIG_USB_XHCI_IMX8 = n
2) device tree: GPU Clock down
& gpu_3d0 {
-assigned-clock-rates = <700000000>, <850000000>;
+ assigned-clock-rates = <372000000>, <372000000>;
Besides this, Ether is also changed to 1G-> 100M. Do we need to modify the device tree for this?
If so, how should it be corrected?
If there are other points that need to be corrected, please let me know.
BR,
Kanou
解決済! 解決策の投稿を見る。
Hello,
Could you please submit a case?
There is some information that could not be shown here.
Best regards,
Diego.
Hello,
Could you please submit a case?
There is some information that could not be shown here.
Best regards,
Diego.