How to handle unused pins? (e.g. GPIO, PCIe, SD-card.....)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to handle unused pins? (e.g. GPIO, PCIe, SD-card.....)

1,084 Views
bjoern_harre
Contributor I

Is there any application note with information about how to handle unused pins? If they shall be left unconnected or connected to an pull-up or pull-down resistor.

Labels (1)
Tags (1)
0 Kudos
3 Replies

993 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bjoern Harre,

How to handle unused pins difers a little depending on the processor and module. All Hardware Design Guides for i.MX Processors have recommendations and directions for unused interfaces. Hence, I would recommend that you look for the Hardware Design Guide for your processor on the NXP website. If you have trouble finding it please just let me know which i.MX Processor you are using and I can point you to the right document.

I hope this helps!

Regards,

0 Kudos

993 Views
bjoern_harre
Contributor I

Yes, it helps a bit. I find a few infos in ths document: IMX8MMHDG. My favourite CPU is: MIMX8MM6DVTLZAA.

But what about the following interfaces/signals for :

- SD1 interface

- NAND

-SPDIF

- JTAG

- CLKIN 1/2 (H27/J27)

- CLKOUT 1/2 (H26/J26)

Br

Bjoern

0 Kudos

993 Views
mrudangshelat1
Senior Contributor II

Hi Bjoem,

My suggestion as below.

- SD1 interface: Floating / Terminate on Test Point for future interface

- NAND: Floating

- JTAG: Terminate on Test point for debugging purposes. Use Pullup/Pulldown resistors where it is required on signals.

- CLKIN 1/2 (H27/J27): Terminate on Test point

- CLKOUT 1/2 (H26/J26): Terminate on Test point

pastedImage_1.png

Regards,

Mrudang

0 Kudos