How to enable OTG2 to USB device mode in i.MX6 solo lite CPU ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable OTG2 to USB device mode in i.MX6 solo lite CPU ?

3,588件の閲覧回数
Danube
Contributor IV

Hi All,

How to enable OTG2 to USB device mode in i.MX6 solo lite CPU ?

We had check with driver , OTG1 is OTG mode and OTG2 is fixed in USB Host mode.

We want to enable USB device only in OTG2

Does any patch can do it ?

ラベル(4)
8 返答(返信)

1,539件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Do you have the part number of the board you are using?

0 件の賞賛

1,539件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

we are using the i.mx6 SABRESD board. You can find the detail info on www.freescale.com

0 件の賞賛

1,539件の閲覧回数
Danube
Contributor IV

Hi Qingrong,

Could you please using MX6SLEVK to test it ?

We are using i.MX6 solo lite CPU. (13mmx13mm package)

0 件の賞賛

1,539件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

I have no MX6SLEVK board in my hand. I only have the MX6DQ board.

From the RM, it seems the OTG2 can't support device mode. Have you test the host mode for it?

1,539件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Can you check attached patch to see if it can help you. It is not for SX. But it can switch USB OTG mode.

1,539件の閲覧回数
MaxChou
Contributor III

11111111111111111111111.png

dear   sir.

      does it mean OTG2 could support device mode or not ?

i can't understand the decription in linux reference manual.

0 件の賞賛

1,539件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

It seems it can't support device mode due to the USB2PCI bridge connected.

1,539件の閲覧回数
MaxChou
Contributor III

dear  Qingrong

thanks for your reply,

where is the USB to PCI bridge?,

it is connect to chip inside ?

0 件の賞賛