Hi Dhanush
if codec is connected via i2c, one can try to read its registers using i2c tools:
https://community.nxp.com/docs/DOC-343682
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
thanks for your reply.
Im stuck at one position from many days,Please can you help me to resolve
the issue.
During the porting of wm8960 codec , Im facing the issue like there is no
clk signals(BCLK,FCLK,Tx) ,except mclk from processor.
Tool chain -- Yocto
BSP -- 4.9.11
Processor -- IMX6UL
Interfaces -- i2c1,sai2
dts interface: