Hi charles
one can try to use asrc please refer to Chapter 29
Asynchronous Sample Rate Converter (ASRC) Driver,
sect.28.5.2 7.1 Audio Codec Unit Test
attached Linux Manual and use dts sabresd examples.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi NXP
Thanks your feedback.
My imx6q platform OS is android 6.0.1. We need the android 6.0.1 solution.
My customer need to change "sample rate" for play and record.
So do you have any solution about change the sample rate in Android 6.0.1.
I try get some log message and when I open Audio APK.
logcat -v time | grep audio
06-23 10:21:43.842 W/audio_hw_primary( 212): do_out_standby... -1242503424
06-23 10:21:49.552 W/audio_hw_primary( 212): out_set_parameters routing=2, ret 0, out -1242503424
06-23 10:21:49.561 I/audio_hw_primary( 212): start_output_stream_primary... -1242503424, device 2
06-23 10:21:49.563 W/audio_hw_primary( 212): card 0, port 0 device 0x2
06-23 10:21:49.563 W/audio_hw_primary( 212): rate 44100, channel 2 period_size 0xc0
The some message form hardware/imx/alsa/tinyalsa_hal.c . (not linux kernel.)
Do you have any advice?
Best regards.