How to connect the printer(e.g. HP Laser Jet P1108)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect the printer(e.g. HP Laser Jet P1108)

1,978 Views
Mihan
Contributor IV

Hi

I want to connet the printer by USB or LAN on IMX6DL.

The rootfs is built normally, so it doesn't have cups,right?

Could I follow the step mentioned in Linux cups | NXP for fsl-yocto-L4.1.15_2.0.0-ga?

On the other hand, Some HP printers need hplip and hplip-plugin.

How to install those into the system?

Regards

Mihan

Labels (4)
Tags (3)
0 Kudos
Reply
3 Replies

1,674 Views
igorpadykov
NXP Employee
NXP Employee

Hi 铭恒 李 

one can follow yocto tutorials:

https://community.nxp.com/docs/DOC-95333 

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,674 Views
Mihan
Contributor IV

Hi

I got cups and hplip by adding IMAGE_INSTALL_append = " cups" and IMAGE_INSTALL_append = " hplip" in local.conf.

but when I run hp-check, there are some errors about missing required dependencies hp-check结果.bmp

some dependencies are not in list

0 Kudos
Reply

1,389 Views
Ryze
Contributor I

I'm have the same problem, do you have any suggestions?

0 Kudos
Reply