Hello,
We would like to configure the SDIO /MMC voltage levels in IMX6 platform. We need to configure 1.8v instead of
3.3.v. Is any kernel configuration / register programming required for this change (or) any iomux register configuration is required to achieve this.
Please any one help with this
Regards,
Siva.
已解决! 转到解答。
Hello,siva,
See following picture:
The above means:
if you use 1.8V voltage at pin NVCC_SD1, The high level on SD1 port will be 1.8V.
if you use 1.8V voltage at pin NVCC_SD2 The high level on SD2 port will be 1.8V.
SD3 and SD4 are the same as SD1 and SD2.
Regards,
Weidong
Hello,siva,
See following picture:
The above means:
if you use 1.8V voltage at pin NVCC_SD1, The high level on SD1 port will be 1.8V.
if you use 1.8V voltage at pin NVCC_SD2 The high level on SD2 port will be 1.8V.
SD3 and SD4 are the same as SD1 and SD2.
Regards,
Weidong
Hi Weidong,
How 's about kerrnel config to make SD port work at 1.8V?
Our board has SD ports that hardware configured to work at 1.8V. But when I use "cat ios" command to check, It show 3.3V as below:
root@android:/ # cat sys/kernel/debug/mmc0/ios
clock: 52000000 Hz
vdd: 20 (3.2 ~ 3.3 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 5 (invalid)
root@android:/ #
Could you give me some suggestion?
Thanks.