How to config audmux between bluetooth and codec

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to config audmux between bluetooth and codec

1,013 次查看
eason
Contributor I

Hi,

How to config audmux between bluetooth sco and codec wm8962 according  different situation.

In our design,

bluetooth  PCM  connect to AUD6.

WM8962 connect to AUD3

CPU already config AUD2 as ssi2.

How to  config AUD6 to AUD2 that using the ssi ?imx_audmux_v2_configure_port??   (The bluetooth sco using the PCM)Is it still SSI ?

Can it dynamic config the audmux when runtime ?Do it need some steps?

标签 (1)
0 项奖励
回复
2 回复数

715 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Hung,

      According to your application, I drew a diagram for you, see following, please !

SSI-AUDMUX-CONFIG.png

(1) Don't need to use second SSI

(2) you should do routing between AUD3 & AUD6

See reference manual, please !

Hope the suggestion can help you !

Regards,

Weidong

0 项奖励
回复

715 次查看
eason
Contributor I

Hi, Weidong

Thank your help.

According your description, I should set the AUDMUX as internel network mode ?

The other problem is SSI config.

In my design ,

BT is slave mode; Codec is master mode ;Which SSI mode  I use?

I search related topic on community , and it maybe set SSI network when use the PCM(BT) ????

0 项奖励
回复