How to change the interface from GRMII to MII on the i.MX6 solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the interface from GRMII to MII on the i.MX6 solo

1,670 Views
coilnpark
Contributor IV

I am developing a module with i.mx6 solo and used 3ports ethernet switch(ksz8873) which includes phys.

Now, I want to change the interface from GRMII to MII on the i.mx6solo.

I guess, I must change the related register, but I am a beginner on the Linux. Can anybody help me?

Labels (2)
2 Replies

1,075 Views
coilnpark
Contributor IV

Hi igor,

Thank you for your help. But, as I said, I am a beginner on the Linux so, I need your step by step explanation.

1. how to change the interface mode from RGMII to MII?

2. In the BSP porting guide file, "In MII mode there are 18 signals defined by the IEEE 802.3 standard" and " Please note that the pin FEC_PHY_RESET_B is used as a simple GPIO to reset the FEC
PHY before enabling phy clock, otherwise some phys will not work correctly."

I want to know whether MII also needs this reset pin or not. 

3. Is there RGMII to MII patch? like you attached patch file. (U-boot + kernel)

Best regards,

Colin

0 Kudos

1,075 Views
igorpadykov
NXP Employee
NXP Employee

Hi Coiln

it is similar to rmii, so one can look at rmii patches

https://community.nxp.com/thread/304346?commentID=331971#comment-331971 

please check Chapter 12 Using the RMII Interface i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

clock should be 25MHz according to sect.4.11.5.1 ENET MII Mode Timing i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------