Hi,
How to changes frequency for usdhc frequency in imx6sx board with kernel version: 4.1.15.
We have custom board based on imx6sx and we are using eMMC with it.
We have changed value in following but changes are not reflected.
File: board/freescale/mx6sxsabresd/mx6sxsabresd.c
API: board_mmc_init
Code :
usdhc_cfg[2].sdhc_clk = 190000000;
printf("DEBUG: Passing new EMMC value 190000000\n");
Output from Linux:
cat /sys/kernel/debug/mmc3/clock
198000000
Is it possible to change eMMC frequency for kernel(or dts file) ?
已解决! 转到解答。
Hi Rakesh
one can try to change usdhc frequency in dcd header
imximage.cfg\mx6sxsabresd\freescale\board - uboot-imx - i.MX U-Boot
use Figure 19-2. Clock Tree i.MX 6SoloX Applications Processor Reference Manual
in linux one can pay attention to "state_100mhz", "state_200mhz" properties
imx6sx-sdb.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
However linux driver sets usdhc frequency automatically based on emmc CSD register
information. May be useful to check :
[PATCH 1/1] mmc: debugfs: Set frequency to maximum possible on higher request
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rakesh
one can try to change usdhc frequency in dcd header
imximage.cfg\mx6sxsabresd\freescale\board - uboot-imx - i.MX U-Boot
use Figure 19-2. Clock Tree i.MX 6SoloX Applications Processor Reference Manual
in linux one can pay attention to "state_100mhz", "state_200mhz" properties
imx6sx-sdb.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
However linux driver sets usdhc frequency automatically based on emmc CSD register
information. May be useful to check :
[PATCH 1/1] mmc: debugfs: Set frequency to maximum possible on higher request
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov:
Thanks for sharing this information.
eMMC frequency changes take effect if frequency is < 100Mhz. For 100Mhz to 198Mhz, it always sets 99Mhz.
root@imx6sxsabresd:/sys/kernel/debug/mmc3# echo 100000000 > clock
root@imx6sxsabresd:/sys/kernel/debug/mmc3# cat ios
clock: 100000000 Hz
actual clock: 99000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 9 (mmc HS200)
signal voltage: 0 (1.80 V)
root@imx6sxsabresd:/sys/kernel/debug/mmc3# echo 190000000 > clock
root@imx6sxsabresd:/sys/kernel/debug/mmc3# cat ios
clock: 190000000 Hz
actual clock: 99000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 9 (mmc HS200)
signal voltage: 0 (1.80 V)
root@imx6sxsabresd:/sys/kernel/debug/mmc3# echo 198000000 > clock
root@imx6sxsabresd:/sys/kernel/debug/mmc3# cat ios
clock: 198000000 Hz
actual clock: 198000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 9 (mmc HS200)
signal voltage: 0 (1.80 V)
Is there any divider need to set anywhere ?