Hello, everyone.
The i.MX53QSB DRAM is 1GB(four chips ddr3, 2 Banks) default.Now, I want to change to 512MB(two chips ddr3 1 Bank).
When I search the method is modify the u-boot-2009.08/board/freescale/mx53_loco/flash_header.S. But I read the assembly code difficulty.
Is anybody can tell me the detail methods? Thank you!
解決済! 解決策の投稿を見る。
You’ll need to adjust board memory size (PHYS_SDRAM_1_SIZE and PHYS_SDRAM_2_SIZE) in include/configs/mx53_loco.h (or appropriate config file for your board).
You'll need to look into ESDCTL register values configured in flash_header.S as they configure memory size but also memory timings, which often need to be adjusted when using different memory compared to what is on the dev. board.
Vladan
You’ll need to adjust board memory size (PHYS_SDRAM_1_SIZE and PHYS_SDRAM_2_SIZE) in include/configs/mx53_loco.h (or appropriate config file for your board).
You'll need to look into ESDCTL register values configured in flash_header.S as they configure memory size but also memory timings, which often need to be adjusted when using different memory compared to what is on the dev. board.
Vladan