Dear all,
I want to add ft5x06 touchscreen driver to match my screen,but I come cross some problem.my system is android 4.3 ,his linux kernel is linux 3.0,35.I want to know how to add the ft5x06 touchscreen driver for my imx6q-sdb to match my screen and which files I should modfy? Thanks!
Hi peng
one can look at sabrelite board :
https://boundarydevices.com/1280x800-displays/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HIigorpadykov
i try to add ft5x506 drvier from boundartdevices,but the x,y position can't mach with screen
can u tell me , how to modify this? tslib ? or?
thx a lot.
Hi igorpadykov
My android BSP is the android_jb_4.3,I have added the touchscreen driver files which is the ft5x06_ts.s and ft5x06_ts.h,and I had modfied the Kconfig Makefile ,and kernel_imx/arch/arm/configs/imx6_android_defconfig,built the uImage and made the bootimage,then download the boot.img to the board ,but I can't find any message about ft5x06_ts in the starting log?According to it ,the driver is invaild,what should I do to deal with it?Thanks!