I'm using an imx6qd board with 2GB DDR, The requirement is to add NOR FLASH support to the board,
The chip I'm using is mt28ew128aba.
I found a file in u-boot "sf_params.c"
And I understand we need to add the i.d in CONFIG_SPI_FLASH_STMICRO
but it requires several fields,
for eg.
{"M25P10", 0x202011, 0x0, 32 * 1024, 4, 0, 0},
what are these values? and where can I find them?
CONFIG_SPI_FLASH_STMICRO is used for serial NOR flash chips. Your chip is parallel NOR with Common Flash Interface (CFI) so you cannot use serial flash drivers to access the chip. You should be using CONFIG_FLASH_CFI_MTD instead. I have not used it myself but there already some boards in u-boot that use CFI flash. You can take those as reference.
Hi Sujay
i.MX6Q Sabre AI board uses M29W256GL7AN6E parallel NOR flash:
mx6sabreauto.c\mx6sabreauto\freescale\board - uboot-imx - i.MX U-Boot
driver description can be found in sect.3.2 EIM NOR Linux Manual.
Best regards
igor
Hi Sujay
one can look at sect.3.8.5 Menu Configuration Options Linux Manual in
Linux 4.19.35_1.1.0 Documentation
Regarding u-boot "sf_params.c" I could not find it in uboot sources
One can pay attention to spi_nor_ids.c :
spi-nor-ids.c\spi\mtd\drivers - uboot-imx - i.MX U-Boot
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------