How to Open LVDS0 and LVDS1 in imx6q for L3.10.53 code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Open LVDS0 and LVDS1 in imx6q for L3.10.53 code?

1,610件の閲覧回数
陳冠儒
Contributor IV

Hi,All:

How to Open LVDS0 and LVDS1 in imx6q for L3.10.53 code?

please help me,thanks.

(中譯 :

  如何打開LVDS0和LVDS1在imx6q上,且用L3.10.53的code

)

ラベル(4)
0 件の賞賛
6 返答(返信)

929件の閲覧回数
陳冠儒
Contributor IV

Hi,All:

Or,

How can the same time output HDMI + LVDS1 in freescale imx6q for L3.10.53 yocto project (linux)?

please help me,thanks.

(中譯 :

  如何可以HDMI+LVDS1  同一時間輸出 在freescale imx6q for L3.10.53 yocto project(linux)?

)

0 件の賞賛

929件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can also look at sect.4.7 Running Linux OS on the target

attached Linux Guide

~igor

929件の閲覧回数
陳冠儒
Contributor IV

Hi,igorpadykov:

thanks for u help.

thanks!!!

But,

Because L3.10.53 BSP (yocto project) is only open fb0 to use, so I can not throw display information to show another fb for dual display.

The L3.10.53 BSP dual display is not the beginning of the same show screen.

Another screen,I must throw things to display,because Framebuffer data is 0.

So,

How to Write freescale imx6q control fb (framebuffer) control program

Or how to control fb?

My experience is not enough, do not know how to write this control program, please help me.

please help me,thanks.

(中譯:

謝謝你的幫忙。

但是,因為 L3.10.53 BSP(yocto project)只打開fb0去使用,所以我不能丟顯示資訊到另一個fb在雙顯示下。

  L3.10.53 BSP 雙顯不是一開始就秀相同的畫面。

另外一個畫面,我必須丟東西去顯示才行,因為Framebuffer 資料是0 。

所以,如何去寫一個freescale imx6q 的控制程式呢?

或者如何去控制fb?

  我經驗不夠,不知道如何撰寫此控制程式,請幫忙我一下。

  請幫助我,感謝。

)

0 件の賞賛

929件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 陳 冠儒

please look at attached Release Notes Table 11.

Common Kernel Boot Parameters for "ldb" parameter options.

Also it may be useful to look at below patch

Re: imx6q and lvds.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

929件の閲覧回数
陳冠儒
Contributor IV

Hi,igorpadykov:

Also ask about,

How to modify the fb device to make the output not only see fb0 (ex:   set the Environment variables :  video = mxcfb0: dev = ldb, LDB-XGA, if = RGB666 video = mxcfb1: dev = hdmi, 1280x720M @ 60, if = RGB24      but  olny see fb0 ouput )?Only to see a display panel (LVDS use  mxcfb0 )output.

please help me,thank.

(中譯:

另外請教一下,

如何修改 fb device 才能讓輸出不只只看到fb0(ex:  設定環境變數 :   video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi,1280x720M@60,if=RGB24  但只看到fb0 輸出)?只看到panel顯示(LVDS 使用 mxcfb0)輸出

)

0 件の賞賛

929件の閲覧回数
陳冠儒
Contributor IV

Hi,igorpadykov:

thanks for u help,I try it.

thanks!!!

0 件の賞賛