Hello community,
Our customer plan to use spread spectrum for System PLL.
Target condition and register setting are following
Target :
Spread spectrum range = 3.52MHz (0.67% of 528MHz →ΔT=0.0126ns→0.5% of 396MHz)
Modulation frequency = 48kHz
Frequency change step = 14.08kHz
Register value:
CCM_ANALOG_PLL_SYS_DENOM[B] = 0x0005B8D8 = 375000
CCM_ANALOG_PLL_SYS_SS[STOP] = 0xD6D8 = 55000
CCM_ANALOG_PLL_SYS_SS[STEP] = 0xDC = 220
CCM_ANALOG_PLL_SYS_SS[ENABLE] = 1b
System PLL condition :
PLL2 = 528MHz
PLL2-PFD0 = 500.21MHz
LDB-DI0 = 71.46MHz = 500.21MHz / 7
Attached figure are spectrum of LDB-DI0 output clock.
Before enable spread spectrum, IMG_0615.jpg
After enable spread spectrum, IMG_0619.jpg
In IMG_0619.jpg, it have three spectrum over 71.46MHz.
Why do spectra occur at high frequencies even though they are down spectrum?
Best regards,
Ishii.
Actually, this spread spectrum mechanism generates the pairs of symmetric spectral frequency harmonics (both upper and lower) around the center frequency of the frequency shift range, i.e. (initial frequency) minus (frequency shift range divided by two), or 71.46MHz - 3.52MHz/2 = 71.46 - 1.76 MHz = 69.7 MHz in your case. So, it's normal to observe the harmonics at the frequencies even upper than the initial one.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------