How should I implement IR enabled on i.MX 8M NANO EVK(8MNANOD4-CPU) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How should I implement IR enabled on i.MX 8M NANO EVK(8MNANOD4-CPU) ?

ソリューションへジャンプ
1,455件の閲覧回数
RabbitThief
Contributor II

Hello,

I'm trying to get IR to work in EVK.

- EVK : 8MNANOD4-CPU

- Linux BSP Version : L5.4.3

I already found the article below through a search, but it keeps failing because the board is different.

IMX8 gpio ir receiver using LIRC 

Up to now, installing LIRC and checking the version has been successful.

Can you please tell me how to edit the .dts file so that the IR GPIO can be set.

0 件の賞賛
返信
1 解決策
1,410件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

unfortunately LIRC and IR are not supported in NXP BSPs, so you should add such support

yourself or apply (if needed) for help to : https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

元の投稿で解決策を見る

5 返答(返信)
1,450件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kisu

 

one can look at example provided on

https://www.imx6rex.com/open-rex/software/how-to-use-access-openrex-peripherals/#ir_rec

 

Best regards
igor

1,416件の閲覧回数
RabbitThief
Contributor II

Hi @igorpadykov ,

I took a closer look at the website you mentioned.

That method was not the Yocto based solution I wanted.

Unfortunately, the directory names and locations didn't work for me, and it was difficult for me to change them.

As already mentioned in the question, the installation of LIRC was successful, and the GPIO settings are not working like the referenced site.

 

Best Regards,

RabbitThief

0 件の賞賛
返信
1,411件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

unfortunately LIRC and IR are not supported in NXP BSPs, so you should add such support

yourself or apply (if needed) for help to : https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

1,407件の閲覧回数
RabbitThief
Contributor II

Hi @igorpadykov ,

I'm going to go ahead with what you told me.

Thanks.

 

Best Regards,

RabbitThief

0 件の賞賛
返信
1,447件の閲覧回数
RabbitThief
Contributor II

Hi @igorpadykov ,

Thank you so much for the information.

I'll give it a try.

0 件の賞賛
返信