How maximum FPC cable distance should I use for MIPI DSI LCD ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How maximum FPC cable distance should I use for MIPI DSI LCD ?

跳至解决方案
1,816 次查看
talel_hajsalem
Contributor III

Hello,

I'm working on a custom IMX8MM board, and I have an LCD display.

when using a 5cm FPC cable and its working, but when using 10cm or 20cm it does not work.

If I decrement the pixel clock it sometimes work.

How maximum length should I don't pass?

Thanks,

Talel

标签 (1)
0 项奖励
回复
1 解答
1,809 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,810 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

0 项奖励
回复