How long time is needed to oscillate i.MX6 external crystals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How long time is needed to oscillate i.MX6 external crystals?

Jump to solution
929 Views
satoshishimoda
Senior Contributor I

Hi, communty,

I have a question about i.MX6DQ external crystals.

Do you know how long times is needed to stabilize the oscillation of external crystals (32.768kHz & 24MHz) from the timing VDD_SNVS_IN is supplied?

Actually, a customer will add delay to POR_B and release POR_B after external crystals oscillation is stable, because reraly i.MX6 cannot boot if POR_B is released before external crystal oscillation.

To understand how much delay should they add, the data is needed.

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
743 Views
Yuri
NXP Employee
NXP Employee

  Hope the app note, linked below helps (assuming typical oscillator considerations

do not depend on processor).

"Practical Considerations for Working With Low-Frequency Oscillators "

http://cache.freescale.com/files/32bit/doc/app_note/AN2606.pdf

View solution in original post

0 Kudos
3 Replies
743 Views
Yuri
NXP Employee
NXP Employee

Oscillator stabilization time depends on environment, schematic, manufacturer and 

may require hundreds msec.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

743 Views
satoshishimoda
Senior Contributor I

OK, I understand depends on many parameter.

BTW, do you have a data of typical oscillation start time of MCIMX6Q-SDP?

And can I calculate the oscillation time with some parameter?

(e.g. benchmark: MCIMX6Q-SDP = 300 msec, oscillation time increase about 10 msec every increase bias resistor 10 ohm)

Best Regards,

Satoshi Shimoda

0 Kudos
744 Views
Yuri
NXP Employee
NXP Employee

  Hope the app note, linked below helps (assuming typical oscillator considerations

do not depend on processor).

"Practical Considerations for Working With Low-Frequency Oscillators "

http://cache.freescale.com/files/32bit/doc/app_note/AN2606.pdf

0 Kudos