hi,
On the software 4.9.88 software, I have configured the ldb node, and the corresponding configuration is as follows:
#############################################################
#include "fsl-imx8qxp-mek.dts"
/ {
model = "Freescale i.MX8QXP MEK";
compatible = "fsl,imx8qxp-mek", "fsl,imx8qxp";
lvds0_panel {
compatible = "boe,av123z7m-n11";
port {
panel_lvds0_in: endpoint {
remote-endpoint = <&lvds0_out>;
};
};
port1{
panel_lvds2_in: endpoint {
remote-endpoint = <&lvds2_out>;
};
};
};
};
&ldb1_phy {
status = "okay";
};
&ldb1 {
split-mode;
/*fsl,dual-channel;*/
status = "okay";
lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
primary;
port@1 {
reg = <1>;
lvds0_out: endpoint {
remote-endpoint = <&panel_lvds0_in>;
};
};
};
lvds-channel@1 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
primary;
port@1 {
reg = <1>;
lvds2_out: endpoint {
remote-endpoint = <&panel_lvds2_in>;
};
};
};
};
&ldb2_phy {
status = "disabled";
};
&ldb2 {
status = "disabled";
};
###################################################################
But can't drive my screen 1920x720p (the timing I have added to panel-simple.c), the error is reported during initialization, the corresponding error message is as follows:
How can I modify if there is an error in configuring the device tree? I hope to get your help, thank you!
LCD screen manual see attachment。
Hi Jinlong
recommended to use Linux L4.14.78 kernel and there is jdi dual-channel LVDS panel example:
i.MX 8QXP MEK Display Selection Guide | NXP Community
seems timings may be adjusted in jdi_tx26d202vm0bwa_timing[]
panel-simple.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If I want to configure uboot show logo, should how to modify?Single an LVDS we can display properly, don't know what to pass kernel parameters, able to provide the corresponding documents?Thank you very much!
logo is configured by #ifdef CONFIG_VIDEO in
uboot//include/configs/imx8qxp_mek.h
imx8qxp_mek.h\configs\include - uboot-imx - i.MX U-Boot
lcd timings by display_info_t const displays[] in
uboot/board/freescale/imx8qxp_mek/imx8qxp_mek.c
imx8qxp_mek.c\imx8qxp_mek\freescale\board - uboot-imx - i.MX U-Boot
Best regards
igor
The above is my configured for single can display properly when an LVDS - 1280 x480, when I change into a double an LVDS screen, don't know how to configure lvds_configure (int lvds_id) function, switch to dual channel an LVDS (SPLIT MODE), how do I configure? In detail how to modify???????????
HI Jinlong:
Are you success to display dual channel lvds(1080p) in kernel ?
I found that , when I set to 1080p, the actual resolution is U:1024x768p-0, I use fsl-imx8qm-mek-jdi-wuxga-lvds1-panel.dts for reference.
Hi Jinlong
NXP has special service for helping with software customizations
NXP Professional Services | NXP
Best regards
igor
Before this I know, because I drive screen is single way an LVDS, already all ok.So also add;Now we use double channel an LVDS driver we screen is there is a problem, can't drive.Is more than the TXT attachment tip error.You said the display of the logo I am an LVDS has shown correctly in a single road, but change the dual channel after an LVDS Gao Qingbing cannot display, driver error...
I have replaced the latest firmware, but also added a timing reference jdi_tx26d202vm0bwa_timing, but start the error ( imx-drm display-subsystem: parent device of /ldb@562410e0/lvds-channel@0 is not available );The corresponding debugging information in the log. TXT inside;Hope to provide some help!