How do I enter Bootstrap mode on an IMX50EVK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I enter Bootstrap mode on an IMX50EVK?

719件の閲覧回数
conorross
Contributor I

What is the dip switch setting for bootstrap mode on the IMX50EVK?

ラベル(1)
0 件の賞賛
1 返信

585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Conor

for bootstrap mode boot pins should be set as:

BOOT_MODE[1:0] =11  - USB Downloader

and one can look at attached EVK schematic p.10

for S1 dip-switch postions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛