Hello
I’m developing a custom board based on QSB now.
This board is implemented connector of i2c.
I want to test the connector to connect the boards to each other.
I want to use in slave mode i2c device. So I would like to use the mxc_i2c_slave.
However, Kconfig is adapted to not read the Kconfig of i2c_slave folder.
Is there a way to use in slave mode of the i2c MX53?
解決済! 解決策の投稿を見る。
There is an example mxc_i2c_slave_test and mxc_i2c_test in the imx-test package in the Linux BSP. You can use this command to extract the source code.
./ltib -p imx-test -m prep
The source code will be extracted to the <ltib>/rpm/BUILD/ folder.
You can take this test code for reference.
There is an example mxc_i2c_slave_test and mxc_i2c_test in the imx-test package in the Linux BSP. You can use this command to extract the source code.
./ltib -p imx-test -m prep
The source code will be extracted to the <ltib>/rpm/BUILD/ folder.
You can take this test code for reference.
I made sure the source code according to your instructions.
I compile and run the source code of these, but the application did not work for / dev/mxc_i2c_slave does not exist.
Is there a way to enable dev/mxc_i2c_slave?
oh, sorry. After look into the i.MX53 QSB BSP driver manual, the I2C driver do not support the I2C slave mode of operation.
So, do you there is no way to use in slave mode in i2c MX53QSB?
Is there a way to improve the mxc_i2c_slave?