Hallo,
I am beginning to work with i.MX28EVK and Linux at all.
How can I change MAC to a new build SD-Card with LTIB?
Under ltib/Package list/boot stream I have found it but can not edit.
"To edit a command line, move the cursor over it and press return." I can see the line but can not edit.
(noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=dhcp gpmi) Default kernel command line for linux_prep
Thanks
Andy
you can use this command to extract the source code
./ltib -p boot_stream.spec -m prep
the source code will be extracted and store in the ltib/rpm/BUILD/.
You can modify the source code. Then type this command to build it again.
./ltib -p boot_stream.spec -m scbuild
Then type this to re-deploy it.
./ltib -p boot_stream.spec -m scdeploy