How Can I boot the SABRE i.mx6 Automotive Infortaintment Development Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How Can I boot the SABRE i.mx6 Automotive Infortaintment Development Board

1,219件の閲覧回数
ahmetkoc
Contributor III

Hi All;

We purchased SABRE main and Cpu board. It has default boot configuration and it has a SanDisk Sd card labeled as Linux 110-77474 C . When We power on the board, there is no response from SABRE card. Main and Cpu board power leds are working properly , ethernet card leds are on during 1 second. After this step there is no response from serial port , ethernet, Hdmi. I could not find any further information on the web. I double checked S1 , S2 and S3 switches, everything seems like ok. Could you give me any suggest ?

My Board Details:

SABRE|Automotive-Infotainment|i.MX6|Freescale

Please check the attachment for my board image.

Best Regards.

Ahmet Koç.

ラベル(1)
タグ(1)
0 件の賞賛
3 返答(返信)

698件の閲覧回数
fabian727
Contributor I

Hi,

were you able to fix your problem? I am stuck at the same point...

0 件の賞賛

698件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Ahmet,

You could try regenerating the bootable SD card, for example, with a newer BSP like Linux 3.14.28. You could download the Linux or Android demo images for regenerating the SD cards using Linux dd command or the MFGtool on Windows. Please refer to the “DEMO_BSPs” downloadable from “Operating System Software-Board Support Packages” section of the following link:

SABRE  Reference Design|Freescale

You could use the Linux dd command in the following way:

    $ sudo dd if=<image name>.sdcard of=/dev/sd<partition> bs=1M && sync

For more information, you could refer to section 6.1 “Flashing an SD card image” of “Freescale Yocto Project User's Guide” document. For the MFGtool usage, please refer to section 4.2.2 “Using MFGTool” of “i.MX Linux User's Guide” document.

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

698件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Additionally, you should ensure the voltage range of the power supply. If you are using just the CPU board, it requires a 5V power supply. However, if using the base board, a 12V power supply is required on this base board.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛