Hi.. i am using a custom board and i have imx6 solo processor on it it works on kernel 3.10 and yacto linux but i want to port android on it. i have tried some prebuild images and burn in sd card not worked can help? thanks in advance
Hi Anupam,
Download android SD demo image from below link and flash it. It will work.
Regards,
Aravinth
Hi..
What I have done I have just change the name of dl to qp . just for information I have a custom board having solo processor on it . now when I boot this board I am geeting no sd card inserted..
Hi Anupam
please look at Android L5 bsps which based on L3.10 kernels.
i.MX 6 Series Software and Development Tool|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ,
Thanks for help as I am new into these can help find the exact BSP. Thanks in advance.
Best Regards,
Anupam Nalgundwar
+91 7083532302
Anacle Systems India Pvt Ltd
S26-S27, Destination Centre 1,
2nd Floor, Nanded City,
Pune: - 411041
Please consider the environment before printing this email.
This electronic message transmission contains information from Anacle Systems Pte Ltd which may be confidential or privileged. Recipients should not file copies of this e-mail with publicly accessible records. The information is intended to be for the use of the individual(s) named above. If you are not the intended recipient, please be aware that any disclosure, copying, distribution or use of the contents of this message is prohibited.
Thanks.. a lot can you tell me is there any document I should refer I have few questions:
1.I have right now linux root fs in EXT3 partion do I need to replace with android rootfs if yes how to do that.
2.with the siurce bsp which you have given I will be able to get the u boot and kernel from it
If you can just provide an overview or any sort of document will be a great help to me…
Thans in advance:)