Hi IMX6ULL14x14EVK OV5640 Camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi IMX6ULL14x14EVK OV5640 Camera

391 Views
ylmzhsn_
Contributor III

Hi NXP,

********

$nano conf/local.conf

CORE_IMAGE_EXTRA_INSTALL += "gstreamer1.0-libav"
LICENSE_FLAGS_ACCEPTED = "commercial"
CORE_IMAGE_EXTRA_INSTALL += " gstreamer1.0-plugins-imx imx-gst1.0-plugin"

******************

$bitbake imx-image-core

Boot:

[ 15.797460] CSI: Registered sensor subdevice: ov5640 1-003c
[ 15.803070] camera ov5640, is found

***********************

$gst-inspect-1.0 | grep "imx"

imx2d: imxpxpvideosink: i.MX PxP video sink
imx2d: imxpxpvideotransform: i.MX PxP video transform
imxaudio: imxuniaudiodec: NXP i.MX uniaudio decoder
imxcompositor: imxcompositor_pxp: IMX pxp Video Compositor
imxmp3enc: imxmp3enc: imx mp3 audio encoder
imxv4l2: imxv4l2sink: IMX Video (video4linux2) Sink
imxv4l2: imxv4l2src: IMX Video (video4linux2) Source
imxv4l2video: imxv4l2videosink: NXP i.MX V4L2 video sink
imxv4l2video: imxv4l2videosrc: NXP i.MX V4L2 video source
imxvideoconvert: imxvideoconvert_pxp: IMX pxp Video Converter
libav: avdec_simbiosis_imx: libav Simbiosis Interactive IMX Video decoder

**************************

$gst-launch-1.0 imxv4l2src device=/dev/video1 num-buffers=1 ! 'video/x-raw' ! jpegenc ! filesink location=/tmp/test.jpg


====== IMXV4L2SRC: 4.7.1 build on Jul 19 2022 06:15:03. ======
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
Redistribute latency...
Got EOS from element "pipeline0".
Execution ended after 0:00:00.982015803
Setting pipeline to NULL ...
Freeing pipeline ...

*************

It saves the captured image to the file path, but the image does not open.Where am I doing wrong?
How do i run ov5640 camera with imx6ull14x14evk. Is there a new document?

0 Kudos
Reply
1 Reply

366 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply